• Max specified Junction Temperature of ADuM5404?

    Dear Sir/Madam,

    What is your Max.specified Junction Temperature of ADuM5404ARW?

    I cannot catch it on your datasheet well.

    Thanks Kaos

  • UVLO min/max of ADuM5404

    Dear Sir/Madam,

    1)As for your ADuM5404, what are your min and max of Vuv+ and Vuv-? As for our reference.....pls let us know.

    2)How can I think this value? Will Min and  Max come form  VIH/VIL correct?

    Thanks Kaos

  • ADuM540x: Automotive version available?

    Do you have an Automotive AECQ Version of the ADUm5401, ADuM5402, ADuM5403,
    ADuM5404

     

    for the automotive version of the ADUM5401 please see the automotive datasheet:

    http://www.analog.com/static/imported-files/data_sheets/ADuM5401W_5402W_5403W…
  • ADM1075 peripheral

    Hello

     

    One of the customer is considering to use ADM1075.

    Referring to UG-548, there are ADuM5404 and ADuM1250.

     

    The customer wants to reduce component count.

    Then they are considering to reduce ADuM1250 and connect as below,

     

       ADM1075      

  • About Viso of ADum5402

    Typical specifications are at TA = 25°C, VDD1 = VSEL = VISO = 5 V. Minimum/maximum specifications apply over the entire recommended operation range which is 4.5 V ≤ VDD1, VSEL, VISO ≤ 5.5 V; and −40°C ≤ TA ≤ +105°C, unless otherwise noted. Switching specifications…

  • RE: I have a question regarding the ADUM5401 EMC;  I am getting a frequency from the switcher at 360MHz; any application of filters used for dampening these frequencies; without having to change the PCB layout.  IE filter circuits

    Gsear: Yes, there are techniques to reduce emissions as suggested in the datasheet:

    ADuM5401/ADuM5402/ ADuM5403/ADuM5404 devices must operate at 180 MHz to allow efficient power transfer through the small transformers. This creates high frequency currents…

  • TAGS LIST: Interface and Isolation

    LTM2894
    LTM2895
    LTM9100
    LTM2885
    LTM2881
    LTM2882
    LTM2883
    LTM2884
    LTM2893
    LTM2886
    LTM2887
    LTM2889
    LTM2892
    LTC1694-1
    LTC4300
    LTC4310
    LTC4302
    LTC4305
    LTC4304
    LTC4303
    LTC4306
    LTC4307
    LTC4307-1
    LTC430…
  • Increasing Available Power of iCoupler devices

    Hello,

     

    In the chapter (page 23) of ADuM5200 datasheet (and in ADuM6200 datasheet too), AD explains how to increase the output power by using 2 devices (one as master and the other one as slave). This is a good thing but it is not as clear (for me…

  • TAGS LIST: Power by Linear

    LTM8045
    LTM8049
    LTM4651
    LTM4661
    LTM4686
    LTM4676
    LTM4686-1
    LTM4676A
    LTM4675
    LTM4677
    LTM4678
    LTM8062
    LTM8061
    LTM8052
    LTM8026
    LTM8056
    LTM8064
    LTM8054
    LTM8055
    LTM4600
    LTM4600HV
    LTM4608A
    LTM4604A
    LTM8032