FAQ
Do you have an Automotive AECQ Version of the ADUm5401, ADuM5402, ADuM5403,
ADuM5404
for the automotive version of the ADUM5401 please see the automotive datasheet:
http://www.analog.com/static/imported-files/data_sheets/ADuM5401W_5402W_5403W…
LTM2894
|
LTM2895 |
LTM9100 |
LTM2885 |
LTM2881 |
LTM2882 |
LTM2883 |
LTM2884 |
LTM2893 |
LTM2886 |
LTM2887 |
LTM2889 |
LTM2892 |
LTC1694-1 |
LTC4300 |
LTC4310 |
LTC4302 |
LTC4305 |
LTC4304 |
LTC4303 |
LTC4306 |
LTC4307 |
LTC4307-1 |
LTC430… |
Typical specifications are at TA = 25°C, VDD1 = VSEL = VISO = 5 V. Minimum/maximum specifications apply over the entire recommended operation range which is 4.5 V ≤ VDD1, VSEL, VISO ≤ 5.5 V; and −40°C ≤ TA ≤ +105°C, unless otherwise noted. Switching specifications…
Gsear: Yes, there are techniques to reduce emissions as suggested in the datasheet:
ADuM5401/ADuM5402/ ADuM5403/ADuM5404 devices must operate at 180 MHz to allow efficient power transfer through the small transformers. This creates high frequency currents…
LTM8045 |
LTM8049 |
LTM4651 |
LTM4661 |
LTM4686 |
LTM4676 |
LTM4686-1 |
LTM4676A |
LTM4675 |
LTM4677 |
LTM4678 |
LTM8062 |
LTM8061 |
LTM8052 |
LTM8026 |
LTM8056 |
LTM8064 |
LTM8054 |
LTM8055 |
LTM4600 |
LTM4600HV |
LTM4608A |
LTM4604A |
LTM8032 |
Hello,
In the chapter (page 23) of ADuM5200 datasheet (and in ADuM6200 datasheet too), AD explains how to increase the output power by using 2 devices (one as master and the other one as slave). This is a good thing but it is not as clear (for me…