• RE: Use ADUM5401 how interface and manegement power

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • (ADuM5401)I have few question about ADuM5401.

    Hi !

    I have few questions about ADuM5401.

    1)=================================================================

    For DC-DC output voltage , the datasheet p3 says the condition is VDD1=5V.

    And Setpoint : Viso Min = 4.7V , typ = 5V,Max = 5.4V.

    Does this…

  • 请问ADUM5401中的high common-mode transient immunity是什么含义?

    这个25K的电压是只哪里到哪里可以承受的电压,是隔离的两端吗?

  • RE: ADUM5401副边没有电压输出

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • ADuM5401 efficiency

    Hello

    Could you show me variation of ADuM5401W efficiency?

    It is available which value is not guaranteed. 

    Tyical value is 30% in the datasheet (P7 Table10).

    I have received query from my customer.

    They have already used the device current model…

  • ADUM5401 and ADM3053: Question Regarding Board Layout to Reduce EMI

    Background:

    • We are using 3 ADUM5401 (RS485 serial) and 1 ADM3053 (CAN bus) to isolate 4 communication ports on a very compact (roughly 8 cm square) 4 layer circuit board with a DSP.
    • We are currently having trouble complying with the radiated EMI…
  • An  issue about ADUM5401

    Dear  Sir/Madam,

    I wonder knowing the meaning of high common-mode transient immunity, and how to test it.

    thanks.

  • ADuM5401 layout question

    we would like to design ADuM5401, but I confused the layout.

    as checked datasheet the air distance is 8.0mm here, I saw the ADuM5401 package is 7.6mm

    what can I do to increase the distance ??

  • Highest allowable overvoultage on ADUM5401

    Hello,

    DIN V VDE V 0884-10 (VDE V 0884-10) INSULATION CHARACTERISTICS

    Highest Allowable Overvoltage     Transient overvoltage, tTR = 10 sec     VTR  up to  4000V peak

                            Who can tell me what's meaning of "tTR", and how to apply the transient overvoltage for 10…

  • what's the curve for CMTI test(ADUM5401)?


    As show above,

    my questions:

    1. what's the centerconductor and shield?

    2.the most important question is :

    what's the curve generated by Pulser? Could you please show me the figure?

    3.what's the curve related to the Vcm=1000V and transient…