• RE: Selecting ADuM5230 Buffer Transistor

    Hello Alex,

    The ADuM5230 has and output current capability based on the size of the internal output MOSFETs. When driving the gate of the IGBT the gate driver is connected to, the amount of current available to drive that gate is limited by the combination…

  • RE: ADUM5230 for Solidtron VCS Drive

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • RE: ADuM5230 for driving AC switch

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • ADuM5230 in a static magnetic filed

    I would like to use the ADuM5230 in a strong static magnetic field and would like to know if there is a limitation from the device in such environment that could be due to the any isolation core material

    Thank you,

  • RE: Is there a eval board for the ADUM5230 ?

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • RE: Problem with ADuM5230 Output going low during static use

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • ADUM5230

    Are there any issues I need to consider if I choose to connect the VAdj to a DAC to control the Isolated supply?

  • [ADuM5230] Clearance and Creepage value is correct? (at Table 4)

    Hello,

    The customer ask about ADuM5230 datasheet description about clearance and creepage value on Table 4.

    This value seems shorter than package size. Is these clearance/creepage value correct?

    It is not same for example ADuM7234 case as below..

  • ADuM5230 with noisy isoGND

    Hi,

    I am trying to use ADuM5230 to function as an AC switch in my resonant converter design.

    The floating ground between two MOSFETs (with back-to-back configuration, having their source as common reference point) is connected to GNDiso, however, with…

  • Ultra Fast Solid State Relay(problems with ADuM5230)

    Hello

    We have a development founded on the ADuM5230.

    Architectural project is a solid state relay (circuit given).

    There is a problem in the ADuM5230.

    If the input is set for a long time a high level, at the output there are occasional dips…