• RE: (ADuM5020 vs ADuM5000W)Do you have one-to-one EMI comparison data?

    Kawa: I don't have a EMI comparison between the ADuM5020 and the ADuM5000.  For the ADuM5020 EMI see the User guide EVAL-ADuM5020EBZ. Emissions on the ADuM5000/ADuM5400 will be shown in the app note AN-0971.

    Regards, Brian

  • Power level of isolated dc-dc converters (with high CMTI)

    I found out that dc dc converters with high CMTI isolation are only available up-to 0.5W of output power (ADuM5000). Are there any other series of products that can go up to 1W?

  • ade9153a

    hi 

    what'is the consuption in current of ade9153a? 

    can i use ADUM5000 dc dc isolator (3.3 to 3.3 isolated) to feed ade9153a and ADUM4152 (spi isolator)?

    IOUT MAX =60mA  ADUM5000

    THANKS

  • Consuption of ade9153A

    Anonymous
    Anonymous

    hi 

    what'is the consuption in current of ade9153a? 

    can i use ADUM5000 dc dc isolator (3.3 to 3.3 isolated) to feed ade9153a and ADUM4152 (spi isolator)?

    IOUT MAX =60mA  ADUM5000

    THANKS

  • RE: CN0349 RF interference?

    If the ADUM5000 is still in place, then don't tie them together. If this test determines that isolation is not necessary, that is, no degradation to your conductivity measurement as a result of shorting grounds, then the next step would be to remove the…

  • RE: Beat frequency when using multiple ADuM5020/5028?

    Hi Minkyun:

    to cancel beat frequency, all the switching power supply must syn the switching frequency. unfortunately, ADuM5020/28 does not have this function. ADuM5000 can be considered. it can be configure to master mode or slave mode. a slave will receive…

  • ADuM5010 Overshoot

    Hi,

    The datasheet of ADuM5000 describes the typical Output Voltage Start-Up Transient
    at 10% and 90% Load, VISO = 5 V in Figure 12.
    We also would like to know that of ADuM5010
    and the maximum output capacitance,

    because we have the overshoot problem in…

  • ADUM5000ARWZ EMI issue

    Has anybody used a ferrite sheet over ADUM5000 to reduce irradiated noise?

  • RE: ADM2587E supply current to external load

    Hi Hiroyuki-san,

    The efficiency is a rough estimate based on the standalone isolated DC-DC product, ADuM5000 (ADM2582E/87E isolated DC-DC is similar). From page 9 of the ADuM5000 datasheet:

    We can see that efficiency with 3.3V to 3.3V is up to 35…

  • RE: CN0349 power consumption

    The CN0349 hardware is no longer available for purchase.

    However, the power dissipation can be calculated by adding up the contributions of the various components as taken from their respective data sheets:

    AD5934 @ 3.3V: 15mA

    AD8606 @ 3.3V: 2.8mA