• ADUM4154 with 2.5V Vdd

    Hi,

    From the ADUM4154 datasheet it looks like Vdd can range from -0.5V to 7V. I figure this is a general range, can this device work with Vdd=2.5V and 2.5V SPI signals? Want to check because all examples are with either 5V or 3.3V.

    Thanks! 

  • RE: 数字隔离芯片ADuM4154ARIZ的测量

    ADuM4154是一款用于SPI隔离的芯片, 并且支持4个SPI Slave的片选。 比较常用的应用场景为模拟信号采集前端或ADC的隔离,满足VDE加强绝缘的要求,如果只是要求基本绝缘,可以选择ADuM3154.

  • TAGS LIST: Interface and Isolation

    LTM2894
    LTM2895
    LTM9100
    LTM2885
    LTM2881
    LTM2882
    LTM2883
    LTM2884
    LTM2893
    LTM2886
    LTM2887
    LTM2889
    LTM2892
    LTC1694-1
    LTC4300
    LTC4310
    LTC4302
    LTC4305
    LTC4304
    LTC4303
    LTC4306
    LTC4307
    LTC4307-1
    LTC430…