I am planning to use Adum3210 isolators between 2 PIC (5Volts, 20-30khz Data Transmission) Should I use serial current limiting resistors before and after ADUM3210? OR should I use no resistor?
I am planning to use Adum3210 isolators between 2 PIC (5Volts, 20-30khz Data Transmission) Should I use serial current limiting resistors before and after ADUM3210? OR should I use no resistor?
Person in charge for IBIS model !
Can you advise me for SIMILAR IBIS model ADuM3210 ?
I am still waiting.
Thanks Kaos
------
Dear Sir/Madam,
Our customer asked as following question.
Do you have the ver1.1 IBIS model for ADuM3210?
There is the…
Hi !
I have some question about ADuM321x.
Q1)
ADuM321x's input signal specification is this.
Is there any Schmitt trigger circuit in this device?
If ADuM32x has, can you tell me the value of hysteresis?
Q2)
Is there AC specification for…
Hi !
I have a question for ADuM321x.
Our customer is thinking to insert ferrite beads to improve EMC tolerance.
Do you have any concern to insert ferrite beads?
The value of the ferrite is not fixed yet.
Best regards.
Kawa
Hi!
I want to know the input capacitance.
At the date-sheet , it says that the typ is 4pF.
But I saw the Ibis-model and also saw figure5 in the application-notes(AN-715).
C_pkg 1.00pF 0.50pF 2.00pF
C_comp 1.00pF 1.00pF 1.00pF
So, my understand…
Dear Sir/Madam,
I have a question for you.
I am studing for our power design.
So I need the supply current for ADuM3210 when this is no communication (=0bps).
Question
What is your minimum current (the quiescient input supply current and the quiescient…
Hello Kaos,
We do have models for the ADuM3210 for both 5 V and 3 V operation:
The ADuM3200 shares the same I/O structures as the ADuM3210 and is offered in the same package, so the…
Hi there,
I have a question about "VDE 0884-10 :2006-12".
According to iCoupler datasheets,
I can find VIORM spec, but I just wondered why each parts has a different VIORM voltage just as following.
(ADuM3210:560V,ADuM2210:846V,ADuM7402…