• ADUM3154 latching output to HIGH when the input is LOW

    Hi all,

    I'm faced with some unpredictible behaviour of the ADUM3154BRSZ-RL7 chip. I'm using this chip for the isolation between temperature measurement ADCs and MCU. SPI bus has 3 MHz SCK. Glitch on MISO line when the initial state was "low" (blue channel…

  • ADuM3154 application that requires isolating two SPI slaves

    1) What is the recommended approach when using only two slaves? We have two /SS pins available from the host MCU. It looks like we should connect the first slave select to /MSS, the second to SSA0, and fix SSA1.  

     

    2) DS table 18, suggests that MI is…

  • RE: 数字隔离芯片ADuM4154ARIZ的测量

    ADuM4154是一款用于SPI隔离的芯片, 并且支持4个SPI Slave的片选。 比较常用的应用场景为模拟信号采集前端或ADC的隔离,满足VDE加强绝缘的要求,如果只是要求基本绝缘,可以选择ADuM3154.

  • SPIsolator(TM) - What is a SPIsolator?

    SPIsolator(TM) are dedicated SPI digital isolators.  We've got your SPI bus covered with the introduction of these 5 new devices:

    The highly integrated ADuM315x SPI digital isolator family simplifies the design of a complete SPI digital isolation…

  • ADE7953 on SPI. Problem with reading registers.

    Hello ADI team

    Started project with ADE7953 and have problem with reading value of it's registers.When write to register (3rd byte in transmission is 0x80), on MISO line receive back it's default value (documentation doesn't say about it), but when want…

  • TAGS LIST: Interface and Isolation

    LTM2894
    LTM2895
    LTM9100
    LTM2885
    LTM2881
    LTM2882
    LTM2883
    LTM2884
    LTM2893
    LTM2886
    LTM2887
    LTM2889
    LTM2892
    LTC1694-1
    LTC4300
    LTC4310
    LTC4302
    LTC4305
    LTC4304
    LTC4303
    LTC4306
    LTC4307
    LTC4307-1
    LTC430…
  • SPI总线在隔离系统中的处理方法

    SPI总线在隔离系统中的处理方法 by ADI_Amy

    SPI(串行外设接口)总线成为设计师宠儿的原因有多种。SPI总线支持高速工作模式,可在短距离内(如电路板芯片间)以最高60 Mbps的速率传输数据。总线在原理上很简单,由一个时钟、两条数据线路和一个芯片选择信号构成。由于数据出现在时钟的一个相位上并在相反相位读回,因此,在速率上出现延迟和失配的几率非常大。最后,总线是由单向线路构成的,这种设计简化了其在微处理器中的实现方式,消除了流程控制问题,非常适合光耦合器或数字隔离器的隔离应用,因为隔离器天生就属于单向器件…

  • SPI总线在隔离系统中的处理方法

    SPI(串行外设接口)总线成为设计师宠儿的原因有多种。SPI总线支持高速工作模式,可在短距离内(如电路板芯片间)以最高60 Mbps的速率传输数据。总线在原理上很简单,由一个时钟、两条数据线路和一个芯片选择信号构成。由于数据出现在时钟的一个相位上并在相反相位读回,因此,在速率上出现延迟和失配的几率非常大。最后,总线是由单向线路构成的,这种设计简化了其在微处理器中的实现方式,消除了流程控制问题,非常适合光耦合器或数字隔离器的隔离应用,因为隔离器天生就属于单向器件。

    在热量或压力监测系统等工业应用中…