• ADUM315x / ADUM3151 / ADUM3152 / ADUM3153 speedgrade question

    Hello together,

    I have a question concerning ADUM315x parts and speedgrade A and B:

    In datasheet you can find the followoing information:

    Later in technical description of the datasheet there are more detailed information;

    So my question why is speedgrade…

  • ADUM3153 Multiple isolators on same spi bus?

    Hi,


    I am experiencing problems using multiple isolators on the same spi bus. I have 8 identical circuits for ade7763's voltage monitors, which each have their own ADUM3153 isolator and own isolated psu, then the common spi bus is connected to the…

  • RE: Digital Isolator for SPI Interface

    Hi Sharvy,

    A  nominal supply voltage of 3.3V or 5.0V will power all SPIsolator Digital Isolators. The ADuM3150/ADuM3151/ADuM3152/ADuM3153 SPIsolator devices will cover your isolation requirement. The ADuM3150 device will support a SPI clock rate up to…

  • ADE7758 Schematic for review

    Hello

    I am designing an energy meter based on ADE7758 and using existing designs for reference (AN-641). The communication between the ADE7758 board and the microcontroller (not shown) is isolated via ADuM3153 SPI isolator. My main concern is about connecting…

  • SPIsolator(TM) - What is a SPIsolator?

    SPIsolator(TM) are dedicated SPI digital isolators.  We've got your SPI bus covered with the introduction of these 5 new devices:

    The highly integrated ADuM315x SPI digital isolator family simplifies the design of a complete SPI digital isolation…

  • TAGS LIST: Interface and Isolation

    LTM2894
    LTM2895
    LTM9100
    LTM2885
    LTM2881
    LTM2882
    LTM2883
    LTM2884
    LTM2893
    LTM2886
    LTM2887
    LTM2889
    LTM2892
    LTC1694-1
    LTC4300
    LTC4310
    LTC4302
    LTC4305
    LTC4304
    LTC4303
    LTC4306
    LTC4307
    LTC4307-1
    LTC430…
  • SPI总线在隔离系统中的处理方法

    SPI总线在隔离系统中的处理方法 by ADI_Amy

    SPI(串行外设接口)总线成为设计师宠儿的原因有多种。SPI总线支持高速工作模式,可在短距离内(如电路板芯片间)以最高60 Mbps的速率传输数据。总线在原理上很简单,由一个时钟、两条数据线路和一个芯片选择信号构成。由于数据出现在时钟的一个相位上并在相反相位读回,因此,在速率上出现延迟和失配的几率非常大。最后,总线是由单向线路构成的,这种设计简化了其在微处理器中的实现方式,消除了流程控制问题,非常适合光耦合器或数字隔离器的隔离应用,因为隔离器天生就属于单向器件…

  • SPI总线在隔离系统中的处理方法

    SPI(串行外设接口)总线成为设计师宠儿的原因有多种。SPI总线支持高速工作模式,可在短距离内(如电路板芯片间)以最高60 Mbps的速率传输数据。总线在原理上很简单,由一个时钟、两条数据线路和一个芯片选择信号构成。由于数据出现在时钟的一个相位上并在相反相位读回,因此,在速率上出现延迟和失配的几率非常大。最后,总线是由单向线路构成的,这种设计简化了其在微处理器中的实现方式,消除了流程控制问题,非常适合光耦合器或数字隔离器的隔离应用,因为隔离器天生就属于单向器件。

    在热量或压力监测系统等工业应用中…