• About ADuM3100

    Hi there,

    I read AD3100 datasheet.

    http://www.analog.com/media/en/technical-documentation/data-sheets/ADUM3100.pdf

    It says that this device is enhanced for ESD protection.

    I just wondered what are the diffrence between other i-coupler products.

  • RE: Noise filter on power line for ADuM1100

    Hi Joseph,

    Yes, it is electrostatic discharge what I say.

    Here is the plan for anti ESD.

    Customer will be put L1, L2 and R1, not LC sorry.

    C1,C2 are coupling capacitor we put in ordinary there closest VDD pin.

    You have ADuM3100 that is more strong…

  • RE: IBIS data for ADUM3210ARZ ,ADUM3100ARZ ,and ADUM3200BRZ

    Hello Kaos,

    We do have models for the ADuM3210 for both 5 V and 3 V operation:

    The ADuM3200 shares the same I/O structures as the ADuM3210 and is offered in the same package, so the…

  • RE: Unidirectional data flow

    Hi:

    The digital isolator can support 3.3V bias and unidirectional communication. please refer to below selection table to search for the right parts.

    the part with 3 digits can support data rate up to 150Mbps.

     PDF

    Regards

    Chris

  • TAGS LIST: Interface and Isolation

    LTM2894
    LTM2895
    LTM9100
    LTM2885
    LTM2881
    LTM2882
    LTM2883
    LTM2884
    LTM2893
    LTM2886
    LTM2887
    LTM2889
    LTM2892
    LTC1694-1
    LTC4300
    LTC4310
    LTC4302
    LTC4305
    LTC4304
    LTC4303
    LTC4306
    LTC4307
    LTC4307-1
    LTC430…
  • Several Issues about AD8251+AD8475+AD7982

    HI,

    I use your company's typical circuit AD8251+AD8475+AD7982 applied to multi-channel acquisition.

    1.The test attachment figure. when the AD8251 input +5V, gain1, AD8475 input +5V, the AD8475 gain is connected to the IN0.4X pin, the AD7982 output…

  • 数字隔离器产品选型与资源指南(2014年春季版)

    产品组合

    • 单通道和多通道数据隔离器

    • 集成隔离电源的数字隔离器:isoPowerRegistered

    • USB隔离器

    • 隔离式栅极驱动器

    • 开关稳压器

    • I2C数字隔离器*

    • 隔离式CAN收发器

    • 隔离式RS-485收发器

    • 隔离式RS-232收发器

    • 隔离式Σ-Δ调制器