• RE: ADUM2251 Side2 Slave don't respond

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • Does ADuM2251 contain magnetic or non-magnetic transformers?

    I'm considering to use this product in very harsh area. The biggest issue is a magnetic field. I'm looking for components which could help to isolate signals, however I cannot use optocouplers or anything sensitive for magnetic field.

  • ADuM2251 static output loading question

    Hello,

    I am using ADuM2250 as I2C isolator, in datasheet recommended operation conditions, it specifys static output loading of minimum 0.5mA, as attached. my question is whether or not it is necessary to maintain more than 0.5mA loading, and what will…

  • ADuM1251 max permitted voltage for IEC 61010 reinforced

    I am getting a little confused. What is the maximum permited voltage under IEC
    61010 for reinforced insulation using this part?

     

    The ADuM2251 is the 5 kV version of that part (ADuM125x is 2.5 kV). The
    certification shows 300 V reinforced…
  • RE: I want to set simple commands in the LMP91000 chip via I2C bus. Does anyone know of a simple USB device I can use?

    Hi TonyF,

    The LMP91000 appears to only have an I2C interface for programming. We'd recommend the ADuM1251 (2.5 kVrms) or ADuM2251 (5.0 kVrms) depending on the withstand voltage requirement for your system.

     

    DaveC

  • RE: Medical I2C Isolation Product?

    Hello,

    The ADuM2250 and ADuM2251 are certified to IEC 60601-1. The RI package with guaranteed 8mm creepage provides the highest approved working voltage.

    FYI, a summary of all digital isolator certifications can be found on the Safety and Regulatory…

  • TAGS LIST: Interface and Isolation

    LTM2894
    LTM2895
    LTM9100
    LTM2885
    LTM2881
    LTM2882
    LTM2883
    LTM2884
    LTM2893
    LTM2886
    LTM2887
    LTM2889
    LTM2892
    LTC1694-1
    LTC4300
    LTC4310
    LTC4302
    LTC4305
    LTC4304
    LTC4303
    LTC4306
    LTC4307
    LTC4307-1
    LTC430…
  • 【在线研讨会讲义下载】了解ADI高性能隔离器解决方案,这个文档就够啦

    近日,ADI 在电子发烧友官网举办了一场在线研讨会【ADI 创新的高性能隔离器解决方案】,向大家展示了 ADI 面向以下应用示例的接口和隔离产品组合:

    • 适合军事和航空航天应用:隔离式 RS-485 收发器

    • 适合高速背板扩展和模拟前端:隔离式 LVDS 产品

    • 适合工业或测试测量系统:隔离式 总线

    • 高度互补的产品组合开创行业最全面的高性能隔离式通信产品套件

    点击链接;http://webinar.elecfans.com/393.html?elecfans_trackid…