• ADUM2211

    Hi

    I have aquestion ADUM2211,

    I think ADUM2211 is 1 to 1 use it .

    If want to use 1 to N(for example , GND2 side to N(1-10 other devices).

    I think cant it is , can you it?

    Best regards

    HOD

  • RE: Hello. i want to know if two outputs of the ADuM2211 can be separated by 400V. In other words if the output of the ADuM2211 are isolated Between them?

    Hi Zoss:

    ADuM2211's outputs are not isolated between each other. I think ADuM3223 or ADuM4223 is suitable for your application.

    its outputs could stand 800Vpeak differential voltage.

    below is the reference diagram for this part.

  • ADUM2211数据异常

    使用adum2211做隔离串口,A SIDE 3.3V ,B SIDE 5V;串口速率19200,出现图片所示问题,但出现这一情况时,双方并没有进行任何通信

  • isolater Maximum Continuous Working Voltage

    Hi

    I have a question , Maximum Continuous Working Voltage.

    This is ADM2484E DS.

    It's written DC Voltage Basic Insulation 1066Vpeak , Reinforced Insulation 529Vpeak.

    ADE7913 DS is , DC Voltage Basic Insulation 1173Vpeak . not have Reinforced…

  • TAGS LIST: Interface and Isolation

    LTM2894
    LTM2895
    LTM9100
    LTM2885
    LTM2881
    LTM2882
    LTM2883
    LTM2884
    LTM2893
    LTM2886
    LTM2887
    LTM2889
    LTM2892
    LTC1694-1
    LTC4300
    LTC4310
    LTC4302
    LTC4305
    LTC4304
    LTC4303
    LTC4306
    LTC4307
    LTC4307-1
    LTC430…