• ADUM2201 PIN14 (VDD) and  PIN 15 (NC) short issues

    Hi All

    I can ADUM2201 pin14 (VDD) and pin 15 (NC) are shorted together to to vcc it?

    This way it will damage the IC?

     

     

  • RE: 5KVrms ADUM2201/ADUM22X

    您可以请参考Mark Cantrell的视频 iCoupler 数字隔离器如何实现8.3mm爬电距离 | 教育 | 亚德诺半导体

    所谓SO8-IC的封装是基于SO8-W的基础上进行的改良,通过增加周长的方式使得iCoupler技术满足8.3mm爬电距离要求

    问题的出发点是:原SO16-W改为现SO8-IC,是否性能/功能完全一致?毕竟十年前的技术和现在相比,ADI可以做得更好

  • RE: ADUM2201BRWZ Case Temperature (Tcase)

    Hi,

    In the datasheet of ADuM2201, you will find the max operation temperature is 105C for B grade. That means the ambient temperature. And the junction temperature is 150C. We don't measure the max Case temperature. But I think the two temperature we…

  • RE: ADUM2201ARWZ IEC60950-1

    Hello Webber,

    I would like to add some detail to the previous discussion.

    CSA60950 can be used for any altitude.  The standard refers the designer to the insulation coordination standard IEC60664-1 which has table A.2 Altitude Correction Factors.  The…

  • TAGS LIST: Interface and Isolation

    LTM2894
    LTM2895
    LTM9100
    LTM2885
    LTM2881
    LTM2882
    LTM2883
    LTM2884
    LTM2893
    LTM2886
    LTM2887
    LTM2889
    LTM2892
    LTC1694-1
    LTC4300
    LTC4310
    LTC4302
    LTC4305
    LTC4304
    LTC4303
    LTC4306
    LTC4307
    LTC4307-1
    LTC430…