Hi I would like create a bus SPI with two ADUM1401 and my master device.
I use like a MISO line VOD output of each ADUM1401.
ADUM1401 ------(VOD)-------|
|
|------(spi bus line MOSI)-------------master device
|
ADUM1401-------(VOD) ------…
Hi I would like create a bus SPI with two ADUM1401 and my master device.
I use like a MISO line VOD output of each ADUM1401.
ADUM1401 ------(VOD)-------|
|
|------(spi bus line MOSI)-------------master device
|
ADUM1401-------(VOD) ------…
Hello,
I want to use ADuM1401 to isolate MCU and ADC.
The supply current of ADuM1401 is 31mA per channel when the frequency is 90Mbps, does it means the input signal current should be 31mA? As SPI driving current is several mA, how can I connect these…
我有三块板使用了 ADuM1401CRW。一边是3.3V,另一边5V,在使用过程中不知道什么原因损坏了两片,输出脚高电平(输入脚有波形)。
请问这个是什么原因可能会引起芯片损坏?电路图如下:
图中AI-5V,在不始用的时候电源是被关闭的。
Hello,
I would like to ask the following question about ADUM1401C and ADUM5402C.
I would use ADUM1401C and ADUM5402C to interface to an SPI bus a section of a circuit which has to be isolated. On the SPI bus are connected also other two devices.
So…
Hello,
About ADuM1401 usage around VDD1 and VDD2.
One customer's application has two modes, normal and backup mode.
In normal mode, ADuM1401 both VDD1 and VDD2 are supplied 5V and 3V. There are no problem.
But when application go to backup mode…
ADUM1401C支持最高90mbps,理论支持spi是45mhz。手册上表明ADUM1401C传输延迟是32ns。半时钟周期必须大于传输延迟的2倍。通过计算支持spi速率是是7.8mhz。也不是45mhz。
请问是这样吗?
Hello,
I'm using the ADUM1401 in an application where VDD1 is up long before VDD2. VID is pulled up to VDD2 and when I monitor this signal during startup I can see it following VDD2 as expected.
When looking at VOD, this signal is high when VDD2…
Hello,
The datasheet say the allowed maximum voltage on ADUM1401 inputs are VDD+0.5V. It looks only +0.5V is allowed on inputs when VDD is down(VDD=0V).
Could anyone pls advice whether a series resistor to limit the current into the inputs will allow…