• :ADI年度贺岁片——ADUM1100数字隔离器使用心得和经验

    最近在做逆变器,功率管IGBT需要隔离,想到变压器隔离,但制作变压器比较麻烦,一致性不强。又想到光耦隔离,但光耦的价格很贵和驱动光耦的电流较大;一次偶然的发现了ADUM1100,速度很快,几乎没有延迟,这个芯片使用必须有良好的屏蔽,而且焊接温度不能太高,有好几次都让我烫坏了,找了半天的原因。总之,使用此款芯片要小心谨慎,采用参数表的指示来进行layout。

     

     

    以下是ADUM1100的介绍:

    ADUM1100是采用iCoupler技术的数字隔离器。该隔离器件将高速CMOS与单芯片空芯变压器技术融为一体…

  • RE: disable adum1310 completely

    MBurke: As I see it, you need to reduce the current consumption of the ADuM1310 on the output side 2 to be much less than the 4mA minimum loop current.  The AD421 is specified for externally available current of 3.25mA, assuming 4mA flowing in the loop…

  • 浅谈数字隔离器件的选型与应用

    关于数字隔离器件的选型与应用的资料分享。

  • 高速数字电路中电子隔离应用技巧

    高速数字电路中电子隔离应用技巧 技术文档分享。

  • RE: 有没有5伏/3.3伏无负载时静态工作电流小于1.2毫安的带隔离器件和相应的应用电路设计

    请问您总共需要几个隔离通道呢?芯片的静态功耗是和通道数目相关的,如ADuM1100(单通道),静态功耗可以满足您的要求。

  • RE: Isolated DC/DC Converter and Signal Isolation

    What you found is one option with 2 digital data channels.

    This is the actually smallest combination available on the market.

    For only one data channel the only option would be a DC/DC only - like ADuM5010 combined with a single channel iCoupler like…

  • ADuM1402:  Is there any specified or typical jitter performance?

    Is there any specified or typical jitter performance? We need to transfer a
    clock signal (MCLK) to the AD7766-2 using the ADuM1402, and this clock should
    have low jitter for optical SNR. Would the speed grade of the ADuM ('a', 'b' or …
  • 数字隔离器产品选型与资源指南(2014年春季版)

    产品组合

    • 单通道和多通道数据隔离器

    • 集成隔离电源的数字隔离器:isoPower

    • USB隔离器

    • 隔离式栅极驱动器

    • 开关稳压器

    • I2C数字隔离器*

    • 隔离式CAN收发器

    • 隔离式RS-485收发器

    • 隔离式RS-232收发器

    • 隔离式Σ-Δ调制器

     

  • 隔离、iCoupler®  技术和 iCoupler 产品常见问题解答

    iCoupler 数字隔离器系列提供隔离与创新特性,采用单封装,是业界种类最齐全的隔离器产品,包括标准数字隔离器、采用isoPower 的数字隔离器、集成PWM 控制器和变压器驱动器的数字隔离器、USB 2.0 兼容型隔离器、隔离式门驱动器、隔离式I²C 数字隔离器、隔离式RS-485 收发器、隔离式RS-232 器件、隔离式Σ-Δ型ADC 以及新近发布的隔离线性误差放大器。因此,几乎任何应用都可以找到合适的iCoupler 产品。

    附件是隔离、iCoupler   技术和 iCoupler 产品常见问题解答…

  • RE: ADI设计峰会讲义分享——过程控制系统

    附件是讲义的PDF文档,欢迎大家下载