• FAQ: "Where can I find documentation related to ADuCM302x or ADuCM4050 software drivers (DFP, BSP)?"

    Using bare metal code can be quick and efficient and might even be necessary at times, but is often not scalable enough. And more often than not, can be a pain to debug! Enter the world of embedded C software drivers that abstract out some of the hardware…

  • How to debug code on ADuCM4050 using CCES? Not the eval kit, but using the MCU on Custom Board

    The UserGuide only provides instructions on how to perform debugging using IAR work bench and J-link. How can the same be achieved on CCES? 

  • Getting incorrect Alignment error while flashing code to ADuCM4050

    Getting below warning while flashing code to ADuCM4050.

    complete log:

    Sat Aug 22, 2020 23:20:06: IAR Embedded Workbench 8.50.4 (C:\Program Files (x86)\IAR Systems\Embedded Workbench 8.4\arm\bin\armproc.dll)
    Sat Aug 22, 2020 23:20:06: Loaded macro file…

  • Write Command in UART Downloader mode (ADuCM4050)

    Hi team,

    I'm using a custom board which includes a ADuCM4050 microcontroller. Everything is fine with hardware and FW code, so I discard any possible issue related with them.

    In this moment, I'm developing a bootloader script in Python following the…

  • RE: ADuCM4050 ADC oversampling decreases resolution after waking up from hibernation

    Hi, I apologize for the huge delay.

    The problem was caused by the ACLK not being retained in hibernation mode. Reconfiguring it solved the problem.

    Best regards,

    Hazael

  • RE: UART data transfer speed & OS support of ADuCM4050

    Hi

    1. I've successfully used the ADuCM4050 UART at 1.5Mbaud on many projects. There are configutration examples for 3Mbaud and 6Mbaud as well, but I've not tried those.

    2. the UART peripheral and associated drivers are operating…

  • UART data transfer speed & OS support of ADuCM4050

    Hi Sir,

    I am using ADuCM4050 in my project. I have below 2 queries:-

    1. What is the data transfer speed of UART in controller ?
    2. Which operating system does this controller support ?

    Thanks in advance!

  • UART data transfer speed & OS support of ADuCM4050

    Hi Sir,

    I am using ADuCM4050 in my project. I have below 2 queries:-

    1. What is the data transfer speed of UART in controller ?
    2. Which operating system does this controller support ?

    Thanks in advance!

  • MasterSlaveLoopback example failed in ADuCM4050 microcontroller

    Hi team,

    I'm using ADuCM4050 microcontroller in a embedded system. Using the MasterSlaveLoopback example project, when it reaches the GetBuffer function, it doesn't wake up from LowPowerState (it's flag is equal to 0).

    Using my own code, I…

  • Problem using UART with ADuCM4050

    Hi team,

    I've been working with ADuCM3029 until a few weeks and I'm using an ADuCM4050 microcontroller right now in a embedded system. Some APIs/drivers are different between them, so I had to update the firmware modifying some functions. However, I found…