• aducm4050

    aducm4050 的例程在哪下载,开发环境mdk5

  • aducm4050

    aducm4050 keil的固件库包在aducm哪下载?不是keil的软件包

  • aducm4050

    aducm4050如何在keil上创建工程,启动文件那些在哪下载,.c在哪下载

  • ADuCM4050 Flash Erase Failing

    Hello,

    I am developing an application for the ADuCM4050 microcontroller on a custom board in CrossCore Embedded Studio (v2.9.2), using the ICE-2000 emulator for debugging via SWD.

    Initially this setup worked well. However, after some use, the board stopped…

  • ADUCM4050 ADC power supply

    Hi EZ,

    I am currently doing a schematic using the ADUCM4050, and his internal ADC, and I would like to know few stuff : 

    • Is that possible to have Vbat_ADC set to a different value than the other Vbat of the microcontroller ? 
    • Is that mandatory to…
  • ADuCM4050 failed erasing sectors

    Hello,

    I'm working with the ADuCM4050 on our own board with bare metal SW.

    I used the CrossCore Serial Flash Programmer to program the flash of the ADuCM4050 several times.

    After several successful trials, I continuously receive the following message…

  • ADuCM4050 ADC electrical information

    Hi,

    As far as I looked, I failed to find any equivalent model for an ADC input in the ADuCM4050:

    (analog input) pin capacitance,

    ADC impedance

    I need it in order to be able to calculate the maximum meaningful sampling rate in my circuit.

    Thanks,

    Kob…

  • ADuCM4050 SensorStrobe inputs

    Hi, 

    I need to configure RTC1 and its SensorStrobe channel to interface ADXL372,  ADXL362 or anything similar.

    1)   One INT pin of the accelerometer will be used to provide measurement pulse. So it should be connected to one of the RTC1_SSn pin, is that correct…

  • ADuCM4050 firmware download .

    Hi, 

    I am using a custom made HW. 

    My goal is to use the CrossCore Serial Flash Programmer to download my firmware  to the HW. 

    The problem is that as far as i understand for using the boot kernel i have download my firmware using UART0. 

    On my HW UART0 is not available…