• FAQ: ADuCM360 - IAR Embedded Workbench

    Q.

    Can the IAR Embedded Workbench be used to develop code for the ADuCM360 ?

    -----------------------------------------------------------------------

    A.

    Yes, this no problem. Please find attached the required system-files for installation, a short…

  • LCD interface with ADUCM360

    Dear All,

    I am willing to interface an LCD display (16x2) with ADUCM360 with I2C protocol for display of measured value. 

    Can i have a sample code and recommendation of make for the LCD to have a smoother interface. I tried to connect one LCD display from…

  • ADUCM360 ECLIPSE TOOL CHAIN SUPPORT COMMUNITY

    This community is available for customers looking for support using the customized ADuCM360 Eclipse based IDE. If there are questions pertaining to the tool chain, plugins, or other elements of the IDE, please post your questions/comments here.

     

    The ADuCM360…

  • CN0300: Is it possible to use the ADuCM361 instead of the ADuCM360?

    For CN0300, could the ADuCM361 be used – in other words implement the
    temperature readings and DAC feedback control with just one ADC instead of 2?

     

    As the circuit is currently built, if one ADC is used for everything, the DAC
    output…
  • ADUCM360/361:  SINC3 and SINC4 digital filter performance vs different ADC sampling rates

    Could you provide any further information on the SINC3 and SINC4 digital filter
    performance
    vs different ADC sampling rates?

     

    We provide a worksheet that allows you to enter the Sinc filter and averaging
    filters value you
    want…
  • ADUCM360 IAR J-LINK ERROR

    Hello everyone,

    I'm uploading a program to aducm360 via j-link. But after removing and plugging the usb cable, the program is deleted or does not register. I have to install it again. I think there is a problem with the IAR settings. I would be glad…

  • ADUCM360 IAR CONFIGURATION SETTINGS HELPPPPPPPPP

    Hi,

    I am working on EVAL-ADUCM360MKZ. I downloaded a demo blink project. This file have 3 files inside

    In arm,this is for KEIL. My KEIL version is 5.34.0.0. This project runs smoothly with KEIL. In IAR file, this is for IAR. My IAR version is 8.0. I…

  • ADUCM360 Power Modes. Is the 24Bit-ADC still working in power mode 4 (TOTALHALT)?

    I'm wondering, if the internal 24-bit ADC is still working in Power Mode 4 (TOTALHALT)

    Information about that is missing in Userguide and datasheet.

    In which Power Modes is the internal ADC still working?

  • How can I check ADuCM360 registers when debugging with ADICUP360?

    It is possible to check in Eclipse IDE what are the values of the ADuCM360 device registers? This feature comes with installer or needs additional setup?

  • What do I need if I want to do further development with the ADuCM360 and CN-0267 reference design?

    What do I need if I want to do further development with the ADuCM360 and
    CN-0267 reference design?

     

    If you want to do additional development work you will need a Cortex M3 core
    development
    Kit. You may already have this if you have evaluated…