FAQ
Hi,
would you please let me know what the differences are between ADuCM320i and ADuCM320?
I have a hard time finding this info.
Thanks
Hi,
I am looking for a configuration example to send several spi transactions (let's say a packet of 240 bytes) through dma where chip select should be toggled each 3 bytes. Any example is welcome.
Thanks
(1) Jlink download Firmware into AducM320 by the Jlink with serial SWDIO and SWCLK
(2) after ADucM320 running well, then try to download updated Firmware in the ADucM320 again, while can not download whatever the P2.3(BM) setting high or lower
just popup…
An issue has been identified with MDIOWSD v0.1 supplied on the evaluation DVD.
This issue presents itself as a verify error when certain hex files are downloaded.
The issue has been fixed in the latest version which is avalable from ftp://ftp.analog.com…
想请教一下PLA是怎样工作的,并且PLA_DIN0和GPIO INPUT灌入什么数据,两个信号有关系吗?
最近项目上使用了一个ADUCM320芯片,烧写正常,但是最近采购芯片的时候采购成ADUCM320I,发现程序烧写不进去,但是看手册只有下载接口那块有区别,一个是mdio,一个是i2c,但是我下载的时候用的都是SW接口,按理说不应该出现烧写不进去的问题。现在发现ADUCM320的FLASH地址0x407e8读取出来的信息和ADUCM320I的不一样是,是不是ADUCM320I,我买到假芯片了。
读取出来的数据截图如下:
aducm320I:
aducm320:
Hi Sir,
We us the formula " T = ((VADC-1290)/4.394)+25 " However, always we calculated all negative temperature degree C
For example,
(a) AD22 value : 20000
((20000*(2500/65536))-1290)/4.394+25 = -95 ??
(b) AD22 value : 26500
((26500*(2500/65536…
On our micro we enabled vref output bufferB so on pni AIN11 the 2,5 reference voltage is available.
With this voltage we power some analog circuits like NTC's. We are doubting if the internal reference voltage is always 100% equal to the external voltage…