Can ADuC7121 work at -40 degree C?
Hi all
Can i get an aplicatiion note on how i genarate a triangle wave on IDAC 4 on ADuC7121
thanks
Sabin
Hi
i need the pc program for in circuit serial download via i2c for the ADuC7121. Can any one knows where i can find it ?
thanks
Sabin
Can i get code sample to flash data into the uper 64k flash from code running in the low 64k flash ?
thaks
Sabin
On my ADuC7121 evaluation board, i am not able to achieve the datasheet specifications for the IDACs.
When I look at the IDAC output pins with an oscilloscpe, i am seeing an oscillation of +/-100mV at a frequency of ~25khz.
What is causing this?
我正在使用ADUC7121的温度传感器功能,但是我不太清楚要怎么把我采样得到的电压ADC值转换成对应的实际温度值
????????????????????????????????????????
HI ,EVERYONE,
i am using aduc7121's temperature sensor to monitor the working temperature of my product,no i have get the real ADC value of temperature sensor,But,i do not know how to change the ADC value to the actual temperature in °C
Do U have…
HI ,EVERYONE,
i am using aduc7121's temperature sensor to monitor the working temperature of my product,no i have get the real ADC value of temperature sensor,But,i do not know how to change the ADC value to the actual temperature in °C
Do U have…
In addition, this source code is also valid for the following products:
ADuC7023,
ADuC7121,
ADuC7122,
ADuC7124/26
On the ADuC7023, at what voltage on the input pin will a) a rising edge external interrupt be triggered b) a falling edge external interrupt?
The same question applies for the ADuC7121, ADuC7122, ADuC7124 and ADuC7126.