• FEEPRO code on ADuC7039 Eval board

    Hi,

    I used FEEPRO code on my ADuC 7039 eval-board.

    Then I can't load code on my board anymore.

    I think all memorys are protected by FEEPRO code.

    I used FEEPRO = 0xF0000 ;

    How can I solve this problem?

  • Inquiry regrading ADuC7039 Total Gain Error description

    Hello, all

    Now we have inquiry regrading ADuC7039 Total Gain Error description from our customer.

    Please refer to the comment below, and feedback us with your comment.

    On Table 1. of datasheet page 4, the Total Gain Error for Voltage Channel is defined…

  • We need sample code of the battery sensing for ADuC7039.

    Hi Sir,

    We need sample code of the battery sensing for ADuC7039.

    Because we saw the ADuC7039 is battery sensing/management for automotive systems.

    So we need the sample code that will speed our design process.

    Thanks.

  • 关于ADUC7039光盘资料

    有没有人能给小弟直接发一份啊,上ftp上不去,谢谢了

    邮箱:penghuizou@163.com

  • Flash/EE memory programming via LIN-protocol6 for ADuc7039

    dear sir,

    I am trying to flash code in aduc7039 through LIN using AN946 application,  with MCV combi dongle kit using  LINBWSD.EXE software application.

    the software LINBWSD.exe is showing status as programed successfully (no errors) but after i reset…

  • ADuC7039 - the difference of SPICON.4 and SPICON.9

    Hello!

    I would like to share my problem related to setup of SPI communications with ADuC7039.

    The biggest difficulty for me was to find a proper setup of MISO output enable bits.

    I think that description of SPICON register bits in datasheet is incomplete…

  • RE: Measuring the Current Through sigma delta ADC in ADUc7039

    Dear Sir,

    I am trying to establish LIN communication in ADUc7039. I have desined LIN master and was able to communicate in ADuc7033 but not able to communicate in ADUc7039 can u please help in in this regards.

    In how to configure ADUc7039 as slave and…

  • AD Sampling of ADuc7039 Chip Needs External Reset,how to solve it?

    When I using ADUC7039, Iam found that the system needs external reset after power Down or restart, otherwise the sampling voltage acquisition is incorrect.

    By observing that the AD sampling voltage acquisition is twice the correct value, (For example…

  • ADuC7039单片机进入休眠JTAG无法下载程序

    ADuC7039单片机测试休眠功能,单片机进入休眠后,JTAG丢失与单片机链接,这是正常现象,但JTAG再无法下载,重启复位单片机和JTAG仿真器,JTAG仿真器无法读取CPU的IP,也无法下载程序!

    数据手册讲到单片机休眠后,只有定时器、上电复位和LIN通讯能唤醒;(我个人理解,单片机进入休眠JTAG无法仿真属于正常,但应该能够下载程序,因为JTAG下载的优先级高)

    这问题怎么解决?再者如何调试休眠功能?