• RE: aduc7039 上电需要外部复位,否则AD电压采样不正确

    In the process of using ADUC7039, it is found that the system needs external reset after power Down or restart, otherwise the sampling voltage acquisition is incorrect.

    By observing that the AD sampling voltage acquisition is twice the correct value, …

  • ADuC703x: What is the minimum width of an external Reset Pulse?

    Hi all.

    I was looking for a specification of the minimum pulse width of the external reset of ADuC7036 and ADuC7039.

    However, I could not find.

    What is the minimum width of an external Reset Pulse?

    Best Regards
    aimPoint.

  • (AD8206/AD8211)Why did you change the datasheet?

    Hi !

    I have some questions about ADI datasheet.

    Our team are checking the datasheet because if the datasheet was changed we have to explain the changes.

    And today , we found many datasheet was changed.

    For just one example , AD8206 datasheet was changed…

  • TAGS LIST: Processors & DSP

    ADUC812
    ADUC814
    ADUC816
    ADUC824
    ADUC831
    ADUC832
    ADUC834
    ADUC836
    ADUC841
    ADUC842
    ADUC843
    ADUC845
    ADUC847
    ADUC848
    ADUC7019
    ADUC7020
    ADUC7021
    ADUC7022
    ADUC7023
    ADUC7024
    ADUC7025
    ADUC7026
    ADUC7027
    ADUC…
  • hardware question: is it possible to flash a memory without a debugger ? if so how?

    Hello.

    I have an ADuC7023. Is it possible to download the program to the uC not "through" debugger ??

    I checked the compatibility of ULINK 2 from KEIL, and as can be seen below ADuC7023 is not on that list. That is why I was wondering if…

  • RE: EVAL-ADUC7039QSPZ Evaluation Board Capabilities

    EVAL-ADUC7039QSPZ Evaluation Board Capabilities

    1.) Can ADC sample rate be greater than 1kHz?

    Yes - 8ksps are possible, but for performance and filter capabilities 1ksps are specified and recommended

    2.) Is current shunt included to measure from…

  • RE: Flash/EE memory programming via LIN-protocol6 for ADuc7039

    Please find attached the provisional document including the ADuC7039.

    Regards

    EckartH

  • RE: Debug error in ADuC7020/7026: Unable to halt ARM core

    Please find attached the current version.

  • RE: ADuC7023燒入問題

    建议您参照附件的11页逐一排查