Hi Guys,
would you like to suggest how to convert the obtained value of Temperature in ADC2DAT (ADUc7033) and convert it into the Degree Cenigrades if using internal temperature sensor? Thanks a lot!
Best Regards!
Aaron
Hi Guys,
would you like to suggest how to convert the obtained value of Temperature in ADC2DAT (ADUc7033) and convert it into the Degree Cenigrades if using internal temperature sensor? Thanks a lot!
Best Regards!
Aaron
Dear sir,
I am trying to convert Temperature in The ADUc7033 using Internal Temperature. But the pproblem i am facing is i am not getting the proper Temperature measured. is there any standard method in converting Temperature or else any other method…
The ADuC7033, in fact the whole family ADuC703x Integrated Battery Sensor (IBS) do not have an on-chip UART based bootloader.
The only way to program them is either via JTAG or the integrated LIN downloader.
Hi Naga,
find attached a document called "Migrating from ADuC7033 to ADuC7039" which lists the main differences between the parts.
Also find attached some very basic LIN slave code example in a Keil-Project.
The code will reply to any PID…
Dear Sir,
I am trying to establish LIN communication in ADUc7039. I have desined LIN master and was able to communicate in ADuc7033 but not able to communicate in ADUc7039 can u please help in in this regards.
In how to configure ADUc7039 as slave and…
Hello.
I have an ADuC7023. Is it possible to download the program to the uC not "through" debugger ??
I checked the compatibility of ULINK 2 from KEIL, and as can be seen below ADuC7023 is not on that list. That is why I was wondering if…
Dear sir,
I want to configure Aduc7039 board as the LIN slave. and i want to transmit and receive the data as per the command sent by the master.
for example i am having 3 frames of PID 0x11, 0x12,0x13, so i want to transmit appropriate data when ever…
ADUC812 |
ADUC814 |
ADUC816 |
ADUC824 |
ADUC831 |
ADUC832 |
ADUC834 |
ADUC836 |
ADUC841 |
ADUC842 |
ADUC843 |
ADUC845 |
ADUC847 |
ADUC848 |
ADUC7019 |
ADUC7020 |
ADUC7021 |
ADUC7022 |
ADUC7023 |
ADUC7024 |
ADUC7025 |
ADUC7026 |
ADUC7027 |
ADUC… |