• TAGS LIST: Processors & DSP

    ADUC812
    ADUC814
    ADUC816
    ADUC824
    ADUC831
    ADUC832
    ADUC834
    ADUC836
    ADUC841
    ADUC842
    ADUC843
    ADUC845
    ADUC847
    ADUC848
    ADUC7019
    ADUC7020
    ADUC7021
    ADUC7022
    ADUC7023
    ADUC7024
    ADUC7025
    ADUC7026
    ADUC7027
    ADUC…
  • RE: Debugging the ADUC7126 not work

    Thanks MMA Sir,

    This is my first time contact ADI product, therefore I still don't know how to set config from ADuC7032 to ADuC7126, could you kindly to help me how to do....!!?

    I will download new version of Keil!! thanks for you suggest....^.…

  • RE: Connection to Xilinx KC705 from AD9625 Eva. Board

    Hi Akira-

    For 4L configuration on AD9625, yes you will need to set register 0x05E = 0x04.  This will provide the data on the four lanes 0-3 by default.  Please confirm with your customer that the expectation of data within the KC705 is also on the 4 lower…

  • hardware question: is it possible to flash a memory without a debugger ? if so how?

    Hello.

    I have an ADuC7023. Is it possible to download the program to the uC not "through" debugger ??

    I checked the compatibility of ULINK 2 from KEIL, and as can be seen below ADuC7023 is not on that list. That is why I was wondering if…

  • ad9832 strange behavior

    Hi! I am trying to build a sine waveform generator using ad9832. I already read the topics here with another people having problems with ad9832 but i didn't find the answer so i decided to post this question as a new one.

    The problem is, that i am…

  • RE: High frequency noise at the output of a 4th order filter

    - We picked the quad because of board real estate problems. Is there any application note to explain the issues that you've mentioned in your reply?

    - re: 10k resistor:   We used the resistor values from a filter design tool. Not sure at the moment…

  • How is the Over-Range flag indicator set on the AD9625?

    What logic is used to flag overrange?  Just clipping?  Is one sample reading code 2048 enough, or is there some quantity that’s needed? 

    For the over-range control bit that is embedded in the AD9625 output data stream, only one sample that is equal to…

  • ADuC7XXX系列常见问题解答

    问题:ADUC7XXX系列的开发方法和开发工具是怎样的?

    答案:ADuC7XXX的开发方法是非常简便的。ADUC7XXX系列提供了三种评估板套件,以帮助用户熟悉ADuC7XXX的开发方法和开发环境。以ADUC7020和ADUC7026为例,一种是EVAL-ADuC7020MKZ,这是一种迷你套件,它包括一块迷你评估板,电源线和串行下载线;另一种是EVAL-ADUC7026QSZ,它包括一块评估板,9V电源,串行下载线,和相应的软件光盘;还有一种是EVAL-ADUC7026QSPZ,它与前一种的区别是包括了一个硬件仿真器…

  • RE: External Memory Disabled warning on new hardware

    Hi Stuart,

    XML matches DMC register values, considering register state one step after exiting DDR_INIT().

    I have attached a DXE that generates the warning output after program is loaded.

    Please rename extention .TXT to .DXE, as .DXE extension caused…