• RE: Aduc7020 compatibility with Aduc7028

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • RE: ADuC7028 Reset timing

    Hi,

    Page 95 of the datasheet shows the reset timing section.

    After the internal reset has been activated the GPIO will go to a tristate condition after one cycle of the internal clock, approx. 25 ns. 

    Regards,

    Michael

  • ADuC7028/ADuC7029 - Is underfill required when using these packages?

    The ADuC7028 and ADuC7029 come in 64-Ball and 49-Ball BGA packages respectively.

    When mounting these devices on a PCB, is underfill required?

  • RE: ADuC7028: Incorrect ADC values when clock is set to 41.78MHz - why?

    Extra information:

    The ADC block is clocked by the system clock as selected via PLLCON[1:0].

    By default this is the 41.78MHz PLL output but, it could be an external clock applied to P0.7.

    ADCCON[12:10] bits select the divide rate for the system clock…

  • Compatibility of  ADUC7020 with 7028

    Currently we are using Aduc7020 in our design.We are planning to change 7020 to 7028. As per datasheet internal architecture of both are same excluding the small difference in number of GPIOs. we are not using ADC& PWM portion of this processor.We want…

  • RE: ADuC7026 ECLK

    If you mean either P0.7 on all ADuC702x in general and pin E7 on a ADuC7028, than this is correct, but must be configured that way as explained on page 58.

  • TAGS LIST: Processors & DSP

    ADUC812
    ADUC814
    ADUC816
    ADUC824
    ADUC831
    ADUC832
    ADUC834
    ADUC836
    ADUC841
    ADUC842
    ADUC843
    ADUC845
    ADUC847
    ADUC848
    ADUC7019
    ADUC7020
    ADUC7021
    ADUC7022
    ADUC7023
    ADUC7024
    ADUC7025
    ADUC7026
    ADUC7027
    ADUC…
  • RE: Cannot load Flash Programming Algorithm Aduc7026

    Yeah you're right, it's setup for an aduc7028.

    But it works at my desk with an aduc7026 board. (The 2 devices are from the same family so it doesn't make a difference which one is actually selected).

    I have 2 more suggestions. Do you have…

  • RE: Audc7028 ADC reading issue

    Hi Adam,

    Too early to jump to conclusions based on the evidence presented, the hunt is not over yet!

    I have translated what you have provided to date into assembly code, but cannot see the issue on an ADuC7026 (don’t have an ADuC7028 to hand to try…

  • hardware question: is it possible to flash a memory without a debugger ? if so how?

    Hello.

    I have an ADuC7023. Is it possible to download the program to the uC not "through" debugger ??

    I checked the compatibility of ULINK 2 from KEIL, and as can be seen below ADuC7023 is not on that list. That is why I was wondering if…