FAQ
I find the data sheet of "ADuC7019/20/21/22/24/25/26/27/28/29" can not has detail explanation, How can i find the detail information of the aduc7026 about its registers?
Everything works great except MISO. I'm doing a 4 byte frame and load SPITX after each SPIRx byte is received but only the SPITX byte loaded before the master starts is returned. It is returned 4 times even though I put a new value in SPITX after…
Hi,
Can you check if the board is connected to COM1? If you are using windows, this can be checked at Device manager > Ports
regards,
Mark
Hello,
I Want to Generate 200KHz Square Wave Using The ADuC7026 PWM Module,The Clock Configured for the ADuC7026 is 41.78MHz.
The PWM Initialization Code is:
The Wave Output on the PWM0L is:
That is So Weird!
So,What is the Problem?
Would you like to…