• TAGS LIST: Processors & DSP

    ADUC812
    ADUC814
    ADUC816
    ADUC824
    ADUC831
    ADUC832
    ADUC834
    ADUC836
    ADUC841
    ADUC842
    ADUC843
    ADUC845
    ADUC847
    ADUC848
    ADUC7019
    ADUC7020
    ADUC7021
    ADUC7022
    ADUC7023
    ADUC7024
    ADUC7025
    ADUC7026
    ADUC7027
    ADUC…
  • RE: If using an ADI micorcontroller in a LFCSP package, how do I connect the exposed paddle on the underside of the package on my PCB?

    On the following parts, the exposed paddle is used for mechanical stability and should be connected to a large pad on your PCB but, this pad should not be connected to ground or any other track:

    ADuC7019, ADuC7020, ADuC7021, ADuC7022, ADuC7023, ADuC7024…

  • hardware question: is it possible to flash a memory without a debugger ? if so how?

    Hello.

    I have an ADuC7023. Is it possible to download the program to the uC not "through" debugger ??

    I checked the compatibility of ULINK 2 from KEIL, and as can be seen below ADuC7023 is not on that list. That is why I was wondering if…

  • RE: EVAL-ADuC7020MKZ Mini-Kit Programming/Debug with IAR EWB?

    Here attached now the main part of the Hands-On-Training from 2005.

    The board shown is the regular ADuC7020 board, but it will work the same way with the AduC7020 MiniKIt.

  • 把握黄金急救时间,ADI自动体外除颤器(AED)解决方案免费下载ing!

    你知道心源性猝死(SCD)吗?

    心源性猝死是指急性症状发作后1小时内发生的以意识突然丧失为特征的由心脏原因引起的自然死亡,而且心源性猝死90%以上发生在医院外,但是这类猝死病人的黄金急救时间只有5-10分钟,超过10分钟的抢救存活率不到1%。

    当发生心源性猝死(SCD)时,唯一的救治手段是胸外按压+心脏除颤,及时除颤是迄今公认制止心脏猝死的最有效方法。

    对此,ADI推出了自动体外除颤器(AED)解决方案,可以自动诊断可能危及患者生命的心室纤维性颤动和心室性心博过速两种心律失常症状。

     PDF

    自动一词提示器件可以自主分析患者状况…

  • RE: ADuC7023燒入問題

    建议您参照附件的11页逐一排查