• ADuC7024 PLL Lock

    In the data sheet for the ADuC7024 it says the core stops executing when the PLL loses lock

    "When the internal PLL loses lock, the clock source is removed by a gating circuit from the CPU, and the ARM7TDMI core stops executing code until the PLL regains…

  • ADUC7024/26 通过I2C程序下载问题

    ADUC7024/26通过I2C进行程序下载总是出现错误。

    用的是USB--I2C模块,I2C接口。

    请问这个是什么原因?怎么解决?

  • RE: EVAL-ADXL345Z-DB Micro ADuC7024

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • RE: Reading ADC0 through ADC5 on ADuC7024

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • ADuC7024 Wake-up timer

    Hello, has anyone used the wake-up timer to bring a nap mode ADuC7024 back to its active mode?My testing codes are like below. When I comment out the line “PLL_OSC_CON_EnterPowerMode(OPERATING_MODE_NAP_MODE);”, My LED blinks correctly. However, the LED…

  • USB connection to ADUC7024

    Hello All,

    For my senior project, I will be using the ADUC7024, ADXL345, and various other components to create a fall detection system. I will be designing a custom PCB to meet my design requirements, and I wanted to verify the connection between the…

  • Running RTX on ADuC7024

    Hi. Can any expert give me an example showing how to setup RTX on ADuC7024 using Keil uVision? Based on what I have figured out so far, I understand I need to:

    1. Import the SWI_Handler function (provided by RTX) In my startup file ADuC702x.s

    2. Copy…

  • Keil uVision3 Aduc7024编译错误L6218E

    请问各位专家怎样解决这问题

  • ADUC7024看门狗使用问题

    ADUC的看门狗能不能在看门狗定时没有到之前(即没有复位之前),将看门狗给关了啊?

  • RE: ADuC7024 ADC - Misc questions

    (iv) Writing to ADCCON when a conversion is under way will cause the current conversion to stop and a new conversion to start.

    (v) Same as (iv)

    I'd like to make a correction to (v)

    I found that writing to ADCCP does in fact not restart…