• aduc7020 使用多个定时器中断

    7020能不能使用多个定时器中断?开发板上给了例程但似乎不能运行。

    下面是截取了一部分的例子。将IRQEN定义给TIMER?

    void Timer0Init(void)

    {

    T0LD=163200/128-1;    // 1/128秒中断一次

    T0CON=0xC8;   // Enable Timer0; Periodic mode; FCoreClock/256=163200Hz

    FIQEN |=TIMER0;   //TIMER0中断分配为FIQ

    }

    然后头文件里定义了timer?

  • 关于ADuC7020中温度传感器的问题

    ADcC7xxx系列中说明书说处理器里面有一个温度传感器,该传感器测量芯片温度。

    1、芯片温度和芯片周围的环境是否一样,能否理解为测芯片环境温度?

    2、对于该温度传感器的使用,Keil中通过设置ADCCP=0x10,来实现,那硬件搭线方面需要怎么操作?

    说明书是这样说的,不太理解。

    3、关于该温度传感器的精度,说明书说的是+/- 3摄氏度,那按照电压TC每摄氏度为1.3mv,而ADC转换二进制码对应0.61mV,那应该说精度为0.5摄氏度。是我把精度和分辨率理解错了么。

    期待前辈们解答…

  • An  issue about ADuc7020

    Dear Sir/Madam,


    I am using ADuc7020, when i Invoke  dac.h, appearing below error:

    C:\Keil\ARM\INC\ADI\dac.h(43): error:  #101: "s_DAC_Channel" has already been declared in the current scope

    C:\Keil\ARM\INC\ADI\dac.h:   typedef struct s_DAC_Channel…

  • ADuC7020数模转换、参考电压的问题

    我在使用ADuC7020时,需要产生一个2.5V左右的参考电压,现在我是使用DAC0端口,通过软件设置采用DAC里面的VREF模式在DAC0端输出2.5V电压,通过Keil仿真,可以输出2.5V电压,但是将程序下载到电路板上发现输出端的信号为:

    这个图是通过示波器直接测芯片DAC0输出端的波形,而且该输出端未接任何东西,2.5v电压值正常,但是会出现周期性的毛刺,毛刺大致值为180mV左右。

    我尝试解决问题,首先测芯片供电AVDD,LVDD,均正常,VREF值是正常的,但是也是有同样的毛刺。然后检查其他原因…

  • 关于ADuC7020外部晶振和RST问题求助

    1、我在使用ADuC7020时,在外部晶振上是按照中文说明书上P88页 ,没有在晶振两头放匹配电容,现在使用时发现晶振有时候不能起振,

    想问下放不放匹配电容对起振是否有影响?

    2、关于ADuC7020的端口10(P0.0)和端口19(RST)。P0.0接低电平时擦除程序并下载新程序,而其高电平是运行程序,那我考虑到P0.0悬空时是高电平,P0.0不接电源(高电平)只通过下拉电阻通过开关接地可以吗?对于RST的功能是否是复位键,其接低电平时重新启动不擦除程序,那我RST悬空也可以吧?不知道我的思路和操作是否正确…

  • 关于ADuC7020芯片若干问题请教

       您好,我现在使用贵公司的ARM7芯片ADUC7020BCPZ62,现在有些问题请教:

        (1)关于外部晶振的问题,很多芯片中外部晶振号称芯片的心脏,那在本芯片中不加外部晶振时,芯片是否正常工作,是否只是不能产生外部激励信号源,其他功能还可使用?外部晶振的作用是什么?

         (2)在中文说明书中,说芯片内部集成一个32.768KHz的振荡器,是不是不使用外部晶振振荡器,仍可产生一个32.768KHz信号,只不过精度不太大?

         (3)关于VREF端可产生2.5V电压,还有我使用DAC0端也可产生2…

  • ADUC7020 eval. board software

    I bought ADUC7020 evaluation board. I am looking for ADI ADUC7020 Test Routine Program file.

    Can you tell me what I find that related files?

    David

  • ADuC7020 temperature sensor calculation

    Hello,

    Is there an equation for calculating the the Celcius temperature from the output of ADCDAT?  The example calculation from the ADuC7020 datasheet page 50 is only accurate at room temperature.  As the temperature reaches 80C in the test chamber, the…

  • ADuC7020 P4.0 External Interrupt

    I have observed that P0.4 is an active high IRQ.  Is there any way to configure this to be edge sensitive?  Any example code to do this?

    Thank you, Bob