• Accessing I2C address of ADT7516 ( Temp sensor )

    I have a BBG and EVAL board of ADT7516. I connected them by SDA and SCL pins and as they are to

    be connected with the PC by the usb port, they will have a common ground.

    After this setup, I did i2cdetect -y -r which gives me the output as 0x51.

    This…

  • Device tree bindings for ADT7516

    I have a BeagleBone green and ADT7516's evaluation board connected with SDA and SCL pins.

    When I do i2cdetect -y -r 2, I can see the i2c address as 0x4b and I am able to probe the adt7316 driver present in IIO subsystem.

    adt7316 driver uses platform…

  • Hardware connection failing for ADT7516 sensor ( Driver missing )

    Hello all,

    I have connected the ADT7516 sensor's eval board to my PC through the usb port. Also, I've

    installed the software for it. But it seems that the drivers for the software are missing.

    When I try to run the software with the hardware…

  • ADT7516 Temperature reading update

    I'm having a problem with the temperature reading updates on the ADT7516. The chip is configured for Round Robin operation with external temperature on D+/-. Communications to the chip is through the SPI interface.

    I can get all the temperature and…

  • TAGS LIST: Sensors & MEMS

    ADXL78
    ADXL001
    ADXL278
    ADIS16223
    ADIS16240
    ADIS16209
    ADIS16203
    ADIS16201
    ADXL193
    ADISEVAL
    ADXL1005
    ADIS16000
    ADIS16210
    ADIS16227
    ADIS16228
    ADIS16229
    ADIS16305
    ADXL1001
    ADXL1002
    ADXL1004
    ADXL103
    ADXL151
    A…
  • RE: Customer requires three independent temperature sensors....

    Hi, Unfortunately we don't have any parts in our portfolio that will directly support 3 external temperature channels. Would customer consider muxing three sensors in on D+/D- pins of ADT7516/ADT7517/ADT7519?

  • 2009-08-10 09:17:42     isp1362_hc_reset: Clock not ready after 100ms

    2009-08-10 09:17:42     isp1362_hc_reset: Clock not ready after 100ms

    Chunbo Fan (CHINA)

    Message: 78559   

    hi everyone!

          my target board is ezkit-bf533 and the usb host controller is isp 1362

        // ezkit.c

    #if defined(CONFIG_USB_ISP1362_HCD) || defined…