2010-09-30 10:35:47 temperature sensor
Daniele Pagani (ITALY)
Message: 94070
Dear Sirs,
we're searching for a digital temperature sensore (on the i2c bus) to be used with BF537 and uClinux last release.
Could you suggest something that is…
2010-09-30 10:35:47 temperature sensor
Daniele Pagani (ITALY)
Message: 94070
Dear Sirs,
we're searching for a digital temperature sensore (on the i2c bus) to be used with BF537 and uClinux last release.
Could you suggest something that is…
Hi,
I'm afraid ADT7420 will only allow you to connect 4 devices per bus. On the other hand, if high precision is not a must, you have ADT75 or AD7414, which will allow you up to 8 devices per bus each.
Please find below their datasheets for more…
Original Question: how many number of sensors can be displayed in the monitor? by NagarjunaG
Data corresponding to how many number of sensors is displayed in the ADWSN UI tool?
What if I want interface more sensors in my design, how would I be able to…
Hi,
What I have here is just the output error. I also have 2 more recommendations that are cost-sensitive, the ADT75 and ADT7x10.
Regards,
Karen
Original Question: advantges and disadvantages between the EV-ADRN-WSN-1Z and EV-ADRN WSN-2Z? by ADI_Wei
What are the advantges and disadvantages between the EV-ADRN-WSN-1Z and EV-ADRN WSN-2Z, I don't know which kits should be selected for WSN applications…
Hi Ronald,
The AD7314 is only rated from -35°C to +85°C.
Some devices that may interst you for this project are:
Presenter: Colm Prendergast
Learn how smart partitioning techniques and accurate measurement technologies at the signal chain level can optimize your latest Internet of Things (IoT) application design. Connecting systems on the network edge to cloud…
Dear Blackfin uClinux maintainers,
We're committed to support our ADSP-BF527 powered TLL6527M platform with the Blackfin uClinux distribution. I would like to share update summary on our progress so far.
-> RTC - fine
-> GPIO access - fine…
Original Question: How to recover the setting on EV-ADRN-WSN-1Z by kj.liu
Hi Sir,
First, I got the ADRN-WSN-1Z and the function is ok , but when one of colleague do some change on AnodeCoding and the problem happen. Although the main board still could…
工业WSN系统原理和典型架构
由空间分布式自动传感器构成,用于监控物理或环境条件,如温度、声音、振动、压力、湿度、运动或污染物。以合作方式通过网络将其数据传输到主要地点(基站)。现代WSN具有双向特性,能够同时控制传感器的活动。
WSN由“节点”组成—数量从几个到数百个甚至几千个,其中,每个节点都连接到一个(有时是几个)传感器。每一个这种传感器网络节点一般都包括几个部件:一个无线电收发器,一根内置天线或外部天线连接、一个微控制器、一个传感器接口电路和电源,一般为电池或嵌入式能量采集机制。
…