• ADT75

    I have a problem about ADT75A (SOIC-8).

    When power-up, I read from chip 5 registers:

    TEMP = 0x0000

    CONF = 0x0000

    THYST = 0x0000  (???)

    TOS = 0x5000

    ONESHOT = 0x0000

    Loop (period ~170ms) read from TEMP registers: 0x0000 

    Second board have MAX75…

  • ADT75 ESD and Shelf Life

    What is the ESD rating and shelf life for ADT75?

  • ADT75 internal clk frequency

    Hi


    I would like to know internal clock frequency, and data like PSRR if it can.

    I have a problem.

    ADT75 is mounted on a small board and connected to main board.
    Main board supply the power.
    It must be wire has some registance, I think.
    So power line is…

  • RE: Can ADT75 use "Clock stretch" of I2C standard?

    Hi,

    There is no clock stretching on the ADT75. Can you share what application it is you're working on?

    Regards,

    Karen

  • Does the ADT75 temp sensor require a hardware reset to recover the bus?

    Is it recommended to add a hardware reset to the ADT75 to recover the bus in the event that the active device hangs?

  • RE: ADT7420 (also ADM1176) - Need More than 4 on the same I2C channel!

    Hi,

    I'm afraid ADT7420 will only allow you to connect 4 devices per bus. On the other hand, if high precision is not a must, you have ADT75 or AD7414, which will allow you up to 8 devices per bus each.

    Please find below their datasheets for more…

  • RE: noise floor of the ad22103

    Hi,

    What I have here is just the output error. I also have 2 more recommendations that are cost-sensitive, the ADT75 and ADT7x10.

    Regards,

    Karen

  • Identifying sensors enabled and sensors data, from a data packet of End Point in a network

    Original Question: Identifying sensors enabled and sensors data, from a data packet of End Point in a network by sushma.r

    Hi,

    I have downloaded the ADRadioNet EDK, I have an issues in identifying specific sensor values in the payload displayed on the…

  • FAQ: How to interpret the sensor data collected on ADWSN tool?

    We know the data from different wireless sensors in the network gets collected by the Border Router, and is displayed on the PC monitor using the ADWSN-UI tool. How can this be interpreted - raw data ?

    The sensor data collected on the Border Router…

  • How to interpret the sensor data collected on ADWSN tool?

    Original Question: How to interpret the sensor data collected on ADWSN tool? by NagarjunaG

    I know the data from different sensors gets collected by the Border Router, and is displayed on the PC monitor using the ADWSN-UI tool. I want to know how the raw…