• I2C rise time at 100KHz (ADT7410)

    Hi

    We are using the ADT7410 on an I2C bus with several other I2C devices.
    Our bus runs at 100 KHz (standard mode).
    The SCL/SDA rise time for ADT7410 is quoted at 0.3uS for 0-400Hz on the
    datasheet.
    All of our other I2C devices and indeed the I2C standard…

  • What are the differences between ADT7410 Models

    Hallo

    I`ve looked at the datasheet & found out that this sensor is available in 3 models:

    1. ADT7410TRZ
    2. ADT7410TRZ-REEL
    3. ADT7410TRZ-REEL7

    Could anyone tell me what are the differences between these models?

    Thnx in advance.

  • 关于ADT7410的ack信号无应答

        您好,想利用QuartusII软件,利用FPGA读写ADT7410芯片。因此我的思路是首先对芯片内部相关寄存器进行配置,如地址为0x03的配置寄存器(configuration register),配置为8'b10000001(默认是8'b00000000),因此按照datasheet中的时序图进行编程配置。但是波形的输出中ack始终无应答。如图所示,ccs(第三行的信号)可以当做scl的计数信号,当ccs=0时,让FPGA控制sda在scl为高电平时产生下降沿,作为开始信号。接下来写入10010000…

  • ADT7410的INT引脚上拉电平问题?

    ADT7410的超温中断引脚INT的上拉电平最高是多少V?想用到上拉到+12V,不知可不可以。在datasheet中没有找到。

  • What is the long term temperature drift of the ADT7410?

    I don't see the long term temperature drift in the data sheet and this device is going into a machine with a 7 year life.

    Is there a graph of the drift over time?

  • Connection from ADuCM360 to the ADT7410 via the I2C interface.

    AN-1250 Rev 0, page 5 table 4 mentions .c and .h files for connection from the ADuCM360 to the ADT7410 via the I2C interface. Where to obtain these files?

    The same Application Note mentions on page 1 "See the AN-1250 companion code zip file available…

  • ADT7410 Status Register's Tlow and Thigh bits are never set to '!' as expected?

    I am using the ADT7410's Interrupt mode for INT and CT pins, 13 bits
    resolution, the ID register is '011' for the revision.

    The test is : Ambient temperature is 25°C, with trigger of 27°C, and hysteresis
    of 1°C.
    The chip…
  • 向各位大侠请教一下ADT7410驱动问题

    向各位大侠请教一下ADT7410驱动问题可否使用ADT7420的驱动读取数据?不能的话可否赐小弟一个ADT7410的 驱动程序,谢谢!

  • RE: ADT7420 reportable temperature range

    Should be three to four months.

    I'll stick with the ADT7410 for now.  Thanks for your help.

  • ADT 7410 sample code

    Hi,

          I have purchased ADT7410 ic for my project.Can I get the sample code for this ic?

    Please help.

    regards,

    divya