• How to wake up ADT7301?

    I will use ADT7301.

    It explain about to enter shut down mode in the datasheet.

    I want to know how to wake up.

  • Some issues for DOUT pin of ADT7301

    Hi,       

          My Client used ADT7301, As following is their schematic for ADT7301.

           

           Due to the pull-up resistor, ADT7301 has ~1mA sink current from DOUT pin. Therefore, they have two questions to clarify.

    1. Does this sink current have a chance to damage DOUT…
  • ADT7301 Temp Sensor Digital Output IOL

    The datasheet indicates that for VOL of 0.4V, the Isink = 200uA.   I have a 4.7k pull-up on the DOUT pin and a Vdd of 4.7V.

    This implies I need to sink 1mA, which is not unreasonable.  The datasheet has no chart of Vout vs Iout.

    How much current can DOUT…

  • Diference between adt7301 and adt7311

    Hi,

    I already programmed a microcontroller to use adt7301. Can I use the same code to adt7311?

  • RE: ADT7301 temperature sensor

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • RE: ADT7301, has anyone share source code for Kelvin readout

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • ADT7301 EVAL board documentation and software

    I received this question from a customer:

    Can you tell me if the EVAL-ADT7301EBZ  comes with some sort of driver SW?  I couldn’t find a user’s guide on either the Avnet site nor the ADI site. We are interested in running a unit through our temp chamber…

  • 请问评估板EVAL-ADT7301EBZ要怎么使用?

    评估板EVAL-ADT7301EBZ通过USB连上电脑后,启动ADT7301 Evaluation Software显示,请问该如何解决

  • RE: Question about EVM of AD7814

    Hi JakeKim,

    Would you like to have an evaluation board for testing how the part works? If so, I'm afraid we don't have any evaluation board on this part, but I would suggest to have a look to the following ones, that have the same interface and package…

  • RE: Weird AD7314 behaviour

    Hi, the nearest parts to AD7314 are AD7814 and ADT7301. Eval kits are available for ADT7301.