• Question about ADT6501 current spec.

    Hi Sir,


    My Customer is using ADT6501 in our product and now have some question with it.

    Below is the schematic of ADT6501,

    During the test, we found out that the Vcc of ADT6501 will drop  (dV=429mV) some times when it is working.

    The blue waveform…

  • RE: ADT6401 Output Problem

    Hi, apologies for delay in getting back. We have looked at ADT6401 on the bench and when the rise time is >10mS from 0->2.7V, the part isn’t entering the correct mode with the associated floating inputs.

    We also tied the S2 & S0 pins to Vdd/2 but…

  • RE: need help temp sensor design

    Hi Ronald,

    The AD7314 is only rated from -35°C to +85°C.

    Some devices that may interst you for this project are:

    • The ADT75. This is 2 degree accuracy, i2c interface, digital temperature sensor. It operates between   -55 to +125°C. There is an alert…
  • LM26 alternative

    Q

    Our customer uses this part from TI  : LM26CIM5-HHD .  This has a trip point of
    0 degrees. However , our customer wants a part with a fixed trip point at 7
    degC switch-on? I think that should be p/n LM26CIM5-HSD – but TI do not produce
    such a device…

  • TAGS LIST: Sensors & MEMS

    ADXL78
    ADXL001
    ADXL278
    ADIS16223
    ADIS16240
    ADIS16209
    ADIS16203
    ADIS16201
    ADXL193
    ADISEVAL
    ADXL1005
    ADIS16000
    ADIS16210
    ADIS16227
    ADIS16228
    ADIS16229
    ADIS16305
    ADXL1001
    ADXL1002
    ADXL1004
    ADXL103
    ADXL151
    A…