Q
We're currently laying out a prototype PCB to take an ADSP-TS203 TigerSHARCProcessor (i.e. with only a 32 bit cluster bus and 2 link ports). Could we fit
an ADSP-TS201/2 to this board if we constrict external bus access to 32 bits …
The FIR accelerator on ADSP-SC58x/ADSP-2158x works exactly in the same manner except the following differences:
→ Unlike in ADSP-214xx, you don't need to enable the FIR accelerator in PMCTL1 register explicitly in ADSP-SC58x/ADSP-2158x. In fact,…
The IIR accelerator on ADSP-SC58x/ADSP-2158x works exactly in the same manner except the following differences:
Hi Tingting,
The internal ROM is not user programmable. It is factory programmed, it requires a minimum order and there is an NRE associated for custom ROM programmed parts. For further details please contact your local sales representative.
Best regards…
ADSP-SC58x/ADSP-2158x processors support two options to transfer the data between different on-chip and off-chip memories:
Good day! I have simple question about ADSP-21573/ADSP-SC573. Can external memory controller of ADSP-21573 and ADSP-SC573 work with external SRAM? There is some SMC - this is what we need or it's for something else? We need an analog of AMI from 489 family…
在BF518BF16页面下找到的硬件参考手册当中,封面上写的是Includes ADSP-BF512, ADSP-BF514,ADSP-BF516, DSP-BF518,没有包含518F16 ,也没有勘误表
请问BF518的硬件参考手册和BF518F16有区别吗?
硬件参考手册能使用同一个吗?
Attached memory test can be used to test DDR memory (or any other memory type or memory mapped peripheral) on ADSP-2156x processor. The test is performed for different types of accesses (e.g., core, DMA, 8-/16-/32-/64-bit) and different data patterns…