• prototyping the a ADSP-TS203S design with a ADSP-TS201s or a ADSP-TS202S

    We're currently laying out a prototype PCB to take an ADSP-TS203 TigerSHARC
    Processor (i.e. with only a 32 bit cluster bus and 2 link ports). Could we fit
    an ADSP-TS201/2 to this board if we constrict external bus access to 32 bits
  • ADSP-TS203S and ADDS-PCI-ICE PCI JTAG Emulator

    Hi!

    The ADDS-PCI-ICE PCI JTAG Emulator and VisualDsp++ is full support ADSP-TS203S processor?

    Manufacturer Analog Devices
    Part Number ADDS-PCI-ICE
    SKU 19-07303
  • RE: linkport initialization ts203

    Hi Siddiqui,

    The Link ports in ADSP-TS201 and TS203 are the same you should be able to re-use the Link port codes written for ADSP-TS201 .

    You can refer to this post for reference code

    https://ez.analog.com/message/1993#1993

    Regards,

    Mahesh

  • RE: Kalman Filter Implementation on TS203

    Hi Soobia,

                From your description it is not clear on how you have implemented the Kalman filter on the processor. Do you see the difference between the DSP output and matlab output in terms of some precision or the complete output is wrong? We do not…

  • TS203 TIMER INITIALIZATION

    SIR,

    I NEED TS203 TIMER INITIALIZATION EXAMPLE CODE IN C

    REGARDS

  • DMA Chaining TS203

    Hello,

    I need c example code for DMA  chaining in TS203. 

    Regards

  • Compiler generates unaligned access instructions on a TS203

    Hello all,

    I'm working on a hardware that uses 2 TigerSHARC TS203 revision 2.0. The IDE is the version 5.0 update 10 of Visual DSP++ running on a Windows Vista PC. Optimization settings are at 100% (maximum speed).

    Sometimes the optimiser chooses…

  • use of 64 bit Double data type TS203

    Hello everyone

    Would like to know, how to see the  64 bit  Double variable in VisualDSP++ 4.simulator.

  • Results of Kalman Filter Implemented on TS203 are mismatched with the Matlab results

    Hello ,

    I am facing a problem in implementing Kalman filtering on TS203. The DSP filter results are not matching with matlab result.

    Regards

  • How FFT accelerator (FFTA) on ADSP-SC58x/ADSP-2158x is different as compared to ADSP-214xx processors / What are the major features of FFTA on ADSP-SC58x/ADSP-2158x ?

    FFT Accelerator on ADSP-SC58x/ADSP-2158x is a completely new design as compared to the FFT accelerator on ADSP-214xx processors. The major differences/features of the FFT accelerator on ADSPSC58x/ADSP-2158x are:

    • Unlike in ADSP-214xx, the…