Q
We're currently laying out a prototype PCB to take an ADSP-TS203 TigerSHARCProcessor (i.e. with only a 32 bit cluster bus and 2 link ports). Could we fit
an ADSP-TS201/2 to this board if we constrict external bus access to 32 bits …
FFT Accelerator on ADSP-SC58x/ADSP-2158x is a completely new design as compared to the FFT accelerator on ADSP-214xx processors. The major differences/features of the FFT accelerator on ADSPSC58x/ADSP-2158x are:
Customer ask some questions.
Right now we have plenty of software for ADSP-21489, but it’s quite hard to port it to ADSP-SC573 family. Code itself
is 99% C and C++.
Does family ADSP-SC573 have interface with external static memory like AMI for ADSP…
The FIR accelerator on ADSP-SC58x/ADSP-2158x works exactly in the same manner except the following differences:
→ Unlike in ADSP-214xx, you don't need to enable the FIR accelerator in PMCTL1 register explicitly in ADSP-SC58x/ADSP-2158x. In fact,…
The IIR accelerator on ADSP-SC58x/ADSP-2158x works exactly in the same manner except the following differences:
Hi,
We suggest you to refer "sd_test.c,rsi_test.c" from POST example in below bsp path.
<Installation directory>\ADSP-SC5xx_EZ-KIT_Lite-Rel2.0.2\ADSP-SC5xx_EZ-KIT\Examples\Power_On_Self_Test\common\source
Regards,
Anand Selvaraj.
ADSP-SC58x/ADSP-2158x processors support two options to transfer the data between different on-chip and off-chip memories:
Hi All,
First of all, I already used SigmaStudio for parametric EQ using ADAU1701, never used Sharc tools.
I have a ES9038Pro DAC that work with a USB to I2S converter.
My goal is to interface a ADSP-21489 between the USB to I2S converter and the DAC…