What version of Pads do you need to view the pcb files and schematics of the ADSP-SC589 EZ-KIT evaluation board that you provide for this board .
Regads
Athanasios
What version of Pads do you need to view the pcb files and schematics of the ADSP-SC589 EZ-KIT evaluation board that you provide for this board .
Regads
Athanasios
Hi all,
I'm pleased to announce that we have released a public beta of the 2.0 release of Yocto Linux for ADSP-SC5xx.
The beta release currently contains support for the following development boards:
Other boards will be added…
Hi,
There is no particular EMC Guidelines for ADSP-SC589.
The ADSP-SC589 EZ-Board is in the process of being certified to comply with the essential requirements of the European EMC directive 2004/108/EC and therefore carries the "CE" mark.
We would…
I'm currently using Sigma Studio Version 4.6 Build 0.Rev 1812. I decided to evaluate ADSP-SC589-MINI Evaluation Board, and downloaded SigmaStudioforSharc-SH-Rel2.2.0_Prod and CrossCoreEmbedded Studio-Rel2.10.0. I have installed both of them to Windows…
Hello, I just received my ADSP-SC589 EZKIT and I was wondering if there was some guide on how to port the latest version of LWIP to this platform in bare metal (NO_SYS ==1) mode. LWIP was removed a few years ago. Perhaps if the previous archive was available…
Hello
I didn't find any information about the voltage level to apply on USB_VBUS of the ADSP-SC589. Is 3.3V sufficient?
Best reagrds
Stephane
The attached schematics is the Non-MUX port part of ADSP-SC598.
SYS_CLKIN0, SYS_CLKIN1, CODEC_MCLK_IN ports of ADSP-SC598 are connected to Si5356A-B03215-GM(Attached circuit diagram part number U9).
Can you tell me which parts can replace Si5356A-B03215…
I am designing an interface PCB that will connect to a BRKOUT board attached to an ADSP-SC589 EZ-BOARD. I will use GPIO0-GPIO7 pins to sense a peripheral switch.
Is it necessary to include GPIO pull-up or pull-down resistors on my custom PCB?
Or is it…
Hi!
I am try to use SPI2 in Master mode with DMA.
SPI configured according the CCES example - SPI driver DMA mode.
The problem is that in case of work with one buffer, I got "ADI_SPI_QUEUE_FULL" after the first transaction.
In case of two buffers…
We are working on a custom board design that uses the ADSP-SC589 chip and we would like to make use of the USB1 port as a TTY serial device for U-boot and Linux to use. The USB0 port is already being used to support a hub device. We are using the Yocto…