• How IIR accelerator on ADSP-SC58x/ADSP-2158x is different than the FIR accelerator on ADSP-214xx?

    The IIR accelerator on ADSP-SC58x/ADSP-2158x works exactly in the same manner except the following differences:

    • Unlike in ADSP-214xx, you don't need to enable the IIR accelerator in PMCTL1 register explicitly in ADSP-SC58x/ADSP-2158x. In fact…
  • Is there anything equivalent to External Port DMA (EPDMA) on ADSP-214xx processors available on ADSP-SC58x/ADSP-2158x processors?

    ADSP-SC58x/ADSP-2158x processors support two options to transfer the data between different on-chip and off-chip memories:

    1. MDMA: These are completely new as compared to the EPDMA on ADSP-214xx processors. The programming model of these…
  • ADSP-21573 Second-stage bootloader

    I used the adsp-sc5xx_ez-kit evaluation board to verify that the second-stage loader function,and it can work properly.

    I referred to the demo(SC573_SSL.zip) in the url. ADSP-SC572 Second stage loader won't boot main app with ad-_rom_boot()

    However…

  • ADSP-21573/ADSP-SC573 and external SRAM

    Good day! I have simple question about ADSP-21573/ADSP-SC573. Can external memory controller of ADSP-21573 and ADSP-SC573 work with external SRAM? There is some SMC - this is what we need or it's for something else? We need an analog of AMI from 489 family…

  • ADSP-BF518F16与ADSP-BF518区别?

    在BF518BF16页面下找到的硬件参考手册当中,封面上写的是Includes ADSP-BF512, ADSP-BF514,ADSP-BF516, DSP-BF518,没有包含518F16 ,也没有勘误表

      请问BF518的硬件参考手册和BF518F16有区别吗?

    硬件参考手册能使用同一个吗?

  • ADSP-SC5xx/ADSP-215xx - DDR memory Test

    Attached memory test can be used to test DDR memory (or any other memory type or memory mapped peripheral) on ADSP-2156x processor. The test is performed for different types of accesses (e.g., core, DMA, 8-/16-/32-/64-bit) and different data patterns…

  • ADSP-SC58x/ADSP-2158x Linkport Example code

    Hi,

          Please see the attached example code which allows the link port to be tested on the ADSP-SC589 EZ-KIT. The setup requires the ADSP-SC589 EZ-KIT and the EI3 Probing adapter.

    The attached code configures the link ports in DMA stop mode and transfers…

  • ADSP-BF514 recommended SPI Flash

    Hello,

    Could you please provide a list of recommended external SP Flash ICs for ADSP-BF514KSWZ-4?

    Thanks,

    Evgeny

  • New ADSP-SC58x/ADSP-2158x SHARC Processor Announced!!

    ADI announced today its next generation floating-point SHARC processor, the first dual-core floating-point processor in the portfolio, featuring two improved SHARC+ cores (ADSP-2158x series) and an optional ARM Cortex-A5 core (ADSP-SC58x series). For…

  • Sport issue Between ADSP-SC587 and ADSP-BF561

    Hello,

    ADSP-SC587 interfaced with ADSP-BF561 through SPORT in our custom board, issue is when we set clock frequency 1 MHz communication between the processor is fine. But when we increase  the clock frequency, clock is getting deteriorated. Our requirement…