• ADSP-SC572 Second stage loader won't boot main app with ad-_rom_boot()

    Hi,

    I made a second stage loader for a custom board with an SC572 chipset, but when I try booting from SPI flash using the adi_rom_boot() function it never works.

    I tested that the loader works because when I write to the flash at address 0x00 it boots…

  • Unused DMC pins in ADSP-SC572?

    Has ADI made any progress in documenting what is needed from a hardware standpoint when the DMC is not used? Someone on this forum says don't connect the pins, but does that include DMC_VREF, and 20 pins of VDD_DMC.  Its hard to believe the VDD pins…

  • Cannot connect ICE-2000 to custom board with ADSP-SC572

    We have a custom board with an ADSP-SC572. We've checked what seems to be everything: power rail ramps, reset, clock, and everything seems fine. The ICE-2000 looks like it wants to connect but then we get a FAULT LED on the board and this message in the…

  • 关于Sc572中IIR硬件加速器的使用

    想寻求相关的例程,和matlab滤波器系数的对应关系

  • How FFT accelerator (FFTA) on ADSP-SC58x/ADSP-2158x is different as compared to ADSP-214xx processors / What are the major features of FFTA on ADSP-SC58x/ADSP-2158x ?

    FFT Accelerator on ADSP-SC58x/ADSP-2158x is a completely new design as compared to the FFT accelerator on ADSP-214xx processors. The major differences/features of the FFT accelerator on ADSPSC58x/ADSP-2158x are:

    • Unlike in ADSP-214xx, the…
  • Porting software  from ADSP-21489 to ADSP-21573 and ADSP-SC573 

    Customer ask some questions.

    Right now we have  plenty of software for ADSP-21489, but it’s quite hard to port it to ADSP-SC573 family. Code itself

    is 99% C and C++.

     

    Does family ADSP-SC573 have interface with external static memory like AMI for ADSP…

  • prototyping the a ADSP-TS203S design with a ADSP-TS201s or a ADSP-TS202S

    We're currently laying out a prototype PCB to take an ADSP-TS203 TigerSHARC
    Processor (i.e. with only a 32 bit cluster bus and 2 link ports). Could we fit
    an ADSP-TS201/2 to this board if we constrict external bus access to 32 bits
  • How DMC/DDR controller in ADSP-SC58x/ADSP-2158x different than DDR2 controller on ADSP-2146x ?

    ADSP-2146x

    ADSP-SC58x/ADSP-2158x

    Supports only DDR2 memory devices Supports DDR3, DDR2, and LPDDR memory devices
    Supports maximum clock/data rate of 225/450 MHz Supports maximum…
  • ADSP-SC5xx/ADSP-215xx

    EngineerZone technical forum that provides customer support for Analog Devices ADSP-SC5xx/ADSP-215xx products.
  • How IIR accelerator on ADSP-SC58x/ADSP-2158x is different than the FIR accelerator on ADSP-214xx?

    The IIR accelerator on ADSP-SC58x/ADSP-2158x works exactly in the same manner except the following differences:

    • Unlike in ADSP-214xx, you don't need to enable the IIR accelerator in PMCTL1 register explicitly in ADSP-SC58x/ADSP-2158x. In fact…