• Which difference between ADSP-CM408F-A and ADSP-CM408F-B

    Which difference between ADSP-CM408F-A and ADSP-CM408F-B?

  • 为电机控制领域带来革命性变化——ADI ADSP-CM408F开发套件评测

    为电机控制领域带来革命性变化——ADI ADSP-CM408F开发套件评测 by ADI_Amy

    本文引用自爱板网,原文链接:http://www.eeboard.com/evaluation/adi-adsp-cm408f-eval/

     

        在需要实时信号处理的场合,如电机控制领域,DSP与FPGA都有着广泛的应用。但随着ARM席卷而来,特别是发布了带有浮点运算功能的Cortex-M4处理器之后,ARM也气势汹汹杀入原本DSP占主流的市场。尤其是电机控制领域,一直以来MCU由于性能的限制…

  • ADSP-CM408F 无法下载程序到FLash

    boot mode 每个模式都测试过   J-Link: Flash download: Bank 0 @ 0x18000000: 1 range affected (131072 bytes)

    Thu May 13, 2021 11:03:20: IAR Embedded Workbench 8.30.1 (C:\Program Files (x86)\IAR Systems\Embedded Workbench 8.1\arm\bin\armproc.dll)
    Thu May 13, 2021 11…

  • DAC on ADSP-CM408F Controller

    Hello,

    I want to know if DAC of 12 bit is present in the ADSP-CM408F microcontroller. Looking at the datasheet and user manual which has been written for ADSP-cm40x controllers it is mentioned that there are no DACs availoable for this particular controller…

  • FIR filtering in ADSP CM408F

    Hello,

    I wanted to know if the analog devices processor ADSP-CM408F is capable of doing FIR and IIR filterinig and does it have enough processing power to do it?

    If yes how can you prove it? if not why not?

    Thanks

    Raj lavingia

  • adc on adsp-cm408f unipolar?

    Hello

    Is ADC available on ADSP-CM408F unipolar or bipolar? I tried giving a sine wave signal of 2v p-p and with 0 offset then I got the result shown in the picture attached

    I do not understand the reason behind this clipped sine wave

    Please let me…

  • ADC of ADSP-CM408F Understanding

    Hello,

    I am using ADSP-CM408F internal ADC and using demo examples of ADCC_Circular given by AD. I am using all the newer versions of IAR and trying to get the digital value by running the demo code. Once I load the program into the internal Flash and…

  • Jtag not connected to ADSP-CM408F

    I am using Analog Devices ADSp-CM408F which has arm -cortex m4 chip.

    I am getting an error while compiling a demo code , it says "error while evaluating J link script file" cpu-tap not found in jtag chain

    I have connected the development board…
  • RE: ADSP-CM408F  FREERTOS ADC_circular not working

    Praveen,

    I am using ADSP-CM408F internal ADC and using demo examples of ADCC_Circular given by AD. I am using all the newer versions of IAR and trying to get the digital value by running the demo code. Once I load the program into the internal Flash…

  • FAQ: Is available an elfloader.exe for the ADSP-CM408F?

    Question:

    Is available an elfloader.exe for the ADSP-CM408F?

    -----------------

    Answer:

    The elfloader.exe is not available for ADSP-CM40x series.This is only applicable for Blackfin and SHARC processors.

    This document was generated from the following…