• RE: [BF70X] Deep Sleep mode with USB connection.

    Hello,

    Please find the attached example code for ADSP-BF707 deep sleep which is wakeup by USB wakeup source (WS5).. This code can be directly run in the ADSP-BF707 Ez-Kit and you can understand the working of the code from the comments embedded within…
  • RE: [BF70X] How can I wake up BF703 on Deep sleep by USB?

    Please find the attached example code for ADSP-BF707 deep sleep which is wakeup by USB wakeup source (WS5). This code can be directly run in the ADSP-BF707 Ez-Kit and you can understand the working of the code from the comments embedded within.Please…

  • TAGS LIST: Blackfin Processors

    LABVIEW_EMB_BF
    LABVIEW-SBF
    TOOLS-MISC
    ADSP-BF504
    ADSP-BF504F
    ADSP-BF506F
    ADSP-BF512
    ADSP-BF512F
    ADSP-BF514
    ADSP-BF514F
    ADSP-BF514F16
    ADSP-BF516
    ADSP-BF516F
    ADSP-BF518
    ADSP-BF518F
    ADSP-BF518F16
    ADSP-BF522
    ADSP-BF52…
  • RE: BF703 A boot stream via UART at a speed of 115200

    Yes, if the UART speed is not greater than 57600 the device responds correctly:

      9600 -> <BF 75 00 00> - multicard and motherboard
     19200 -> <BF 3A 00 00> - multicard and motherboard
     38400 -> <BF 1D 00 00> - multicard and mot…

  • CCES 2.6.0 crash at debug start

    Hi all,


    I'm running CCES 2.6.0 from a Windows 8.1 Virtual Machine (VMware) and trying to debug ADSP-BF703 application on my custom target board thru ICE-1000 (v1.2) connected over J2 (10 pins connector).

    Before starting the debug session I see green…

  • [BF70X] Deep Sleep mode with USB connection.

    Dear All.

    I have a question.

    After waking up in Deep Sleep via USB, but the PC can't recognize BF703 by the device manager.

    How can I retain the USB connection after wake up.

    And, is there a way to maintain USB during Deep Sleep Mode?

    And the below…

  • FAQ: CCES 2.6.0 crash at debug start in a Windows 8.1 Virtual Machine

    Question:


    I'm running CCES 2.6.0 from a Windows 8.1 Virtual Machine (VMware) and trying to debug ADSP-BF703 application on my custom target board thru ICE-1000 (v1.2) connected over J2 (10 pins connector). Before starting the debug session I see…

  • Known Errata Against ADSP-BF70x Blackfin+ Datasheet

    We are currently experiencing problems pushing our known documentation errata to the external site, so this Featured Content blurb is going to highlight the known issues:

    1> Table 3 (Clock Dividers) on p14 incorrectly indicates that SCLK0 is "Not available…