As per verification, IBIS model downloaded from website is not working.
Please provide IBIS model of ADSP-BF607.
As per verification, IBIS model downloaded from website is not working.
Please provide IBIS model of ADSP-BF607.
Hi Urmi,
We have IBIS model for ADSP-BF607. Please refer the IBIS model from below link.
www.analog.com/.../ibis-models.html
Regards,
Anand Selvaraj.
Will ADSP-BF607 supports DDR2-800 WHICH WORKS AT 400MHz AT CYCLETIME OF 2.5ns?
Dear All,
Please let me know the maximum speed grade DDR can be supported by ADSP-BF607. Will this support DDR2- 800 speed grade.
Thank you in advance.
Thanks and Regards,
Rohit
Hello,
Please use the below parametric search link to compare the processors
www.analog.com/.../11130
Also, you can look into the the ADSP-BF607 & ADSP-BF523 documentations from below webpage,
www.analog.com/.../adsp-bf523.html
www.analog.com/.../adsp…
Hi Prakash,
Apologies for the delay. Were you able to get going? Please let us know if you are still facing any issues.
Regards,
Anand Selvaraj
thanks for very detailed description, i'll try it !! but the effect also happens if i dont use breakpoints, and only pause core1, then the network seems to be stopped on core0
kind regards christoph
hi !
I'm not sure if we need to use series damping terminators as shown in the ADSP-BF609 EvalBoard.
We are very close to the DSP(BF607) - similar as shown in the eval board - and therefore I don't see the recommendation
to use Rs(series resistors…
I am currently designing with BF607. The USB function will not be used in my design. Is it OK not to power the USB block (i.e. no supply to VDD_USB )? Also, can I leave the unused USB I/O's floating?
Hello,
In my system I have an external signal that generates a pulse every 100us, connected to the NMI input pin of a BF607.
I notice a latency of 1000ns between the falling edge of the incoming NMI trigger and the first line of code within the NMI…