ADSP-BF592: FAQ
Attached is the ADSP-BF592 SPI example code for ADSP-BF592. The connection details are mentioned in the "SPI_TX_RX_Loop.c" file.
Question:
After upgrading to CrossCore Embedded Studio 1.1.0, I can no longer connect to the ADSP-BF592 or ADSP-BF506F EZ-Kit. What’s changed?
---------------------------------
Answer:
CCES 1.1.0 introduces a new driver for the ADSP-BF592 and ADSP…
Hi support team!
I'm trying to use the TWI in the ADSP-BF592, however the TWI option is not appearing in CrossCore "Pin Multiplexing" (FIGURE 1).
Also when I access the "Overview" tab and click on "Add..." I cannot find the TWI for the ADSP…
Q.
How do I use the Tools Utility ROM on the ADSP-BF592?
--------------------------------------------------------------
A.
The ADSP-BF592 introduces the Tools Utility ROM. The Tools Utility ROM contains C Run-Time support routines, the core of VDK and…
Hi Malcolm,
Apologies for the delay.
Can you please let me know the silicon revision of your both old and new ADSP-BF592 Evaluation boards.
Regards,
Anand Selvaraj
Hi,
We suggest you to refer Chapter-16, "Specific Boot Modes" form ADSP-BF59x HRM at below download link.
www.analog.com/.../ADSP-BF59x_hwr_rev1.2.pdf
Regards,
Anand Selvaraj.
Does it means that if the SPORT works in the multichannel mode, the RX and TX channels are synchronous with same clock - RSCLK?
Yes, you are right. The RX and TX channels (of a SPORT) have same clock.
So is that possible to use…
Hi all,
I am using a ADSP-BF592 EZ-KIT Lite board Rev 0.1
with ADI_ADSP-BF592_EZKIT-Rel1.0.0 BSP on Crosscore Embedded Studio 2.11.0.0 (IDE 2.11.56.202204271922)
I have recently installed CCES tools and VisualDSP tools and have settled upon CCES IDE
…