Hello ADI Colleagues,
One of our customers would like to update their hardware with ADSP-21369 to replace ADSP-21363KBCZ-1AA. Do they need to modify their hardware and software?
Thanks & Best regards,
xiangzhi wu
2008-11-02 20:45:01 bf549 EBIU with ARDY access problerm
miaolf miao (CHINA)
Message: 64605
Hi,ALL!
When I set write(read) access cycle =6 sclk(at least 6 sclk), It works ok,But it is too slow, I hope it works fast.
when i set write(read) access…
Target initialization, including system reset, is performed as part of the Cortex-A55 OpenOCD target initialization for ADSP-SC598. If only the SHARC cores are being debugged in ADSP-SC598, a core reset is performed on each loaded core and no system reset…
What are the key differences between the ADSP-SC598 and ADSP-SC594 processors?
2008-06-28 02:08:08 bf549 isp1761 Unlink after no-IRQ error?
miaolf miao (CHINA)
Message: 57979
using isp1760 driver,
#undef MSEC_INT_BASED
16-bit mode.
it return TIMEOUT when usb driver calls
usb_control_msg() to get usb descriptor in hub_port_init…
2008-02-29 21:30:40 Can BF549 use the uClinux that configured for BF548?
joyce jiang (CHINA)
Message: 51939 We got a ADSP-BF548 EZ-KIT Lite,and the EZ-KIT used BF549(and there is a bf535 on the EZ-KIT,I don't know what 's for),I download the latest…
Hi all,
I'm pleased to announce that we have released a public beta of the 2.0 release of Yocto Linux for ADSP-SC5xx.
The beta release currently contains support for the following development boards:
Other boards will be added…
What are the differences between EMAC on ADSP-SC598 processor family as compared to ADSP-SC594 processor family?
What version of Pads do you need to view the pcb files and schematics of the ADSP-SC589 EZ-KIT evaluation board that you provide for this board .
Regads
Athanasios