• On-chip flash for ADSP-BF538F and ADSP-BF539F

    It is mentioned in the data sheet that we need to connect /AMS0 to /FCE to boot
    from on-chip flash.  What should be done with the /FRESET pin?

     

    Typical applications using the Spansion flash device externally would tie
    /FRESET to the system…
  • How many instances does UART have in ADSP-SC59x/ADSP-2159x processor?

    How many instances does UART have in ADSP-SC59x/ADSP-2159x processor?
  • How FFT accelerator (FFTA) on ADSP-SC58x/ADSP-2158x is different as compared to ADSP-214xx processors / What are the major features of FFTA on ADSP-SC58x/ADSP-2158x ?

    FFT Accelerator on ADSP-SC58x/ADSP-2158x is a completely new design as compared to the FFT accelerator on ADSP-214xx processors. The major differences/features of the FFT accelerator on ADSPSC58x/ADSP-2158x are:

    • Unlike in ADSP-214xx, the…
  • Porting software  from ADSP-21489 to ADSP-21573 and ADSP-SC573 

    Customer ask some questions.

    Right now we have  plenty of software for ADSP-21489, but it’s quite hard to port it to ADSP-SC573 family. Code itself

    is 99% C and C++.

     

    Does family ADSP-SC573 have interface with external static memory like AMI for ADSP…

  • prototyping the a ADSP-TS203S design with a ADSP-TS201s or a ADSP-TS202S

    We're currently laying out a prototype PCB to take an ADSP-TS203 TigerSHARC
    Processor (i.e. with only a 32 bit cluster bus and 2 link ports). Could we fit
    an ADSP-TS201/2 to this board if we constrict external bus access to 32 bits
  • RE: How many TRU Interrupts are there for each core in ADSP-SC59x/ADSP-2159x processor ?

    For the ADSP-SC59x/ADSP-2159x set of processors, there are four TRU interrupts from each core.

    TRU Interrupts 0-3 are dedicated to ARM core and TRU Interrupts 4-11 are dedicated to SHARC cores.

  • Does General Purpose Counter in ADSP-SC59x/ADSP-2159x processors detect overflow or underflow in the counter value?

    Does General Purpose Counter in ADSP-SC59x/ADSP-2159x processors detect overflow or underflow in the counter value? 

  • How DMC/DDR controller in ADSP-SC58x/ADSP-2158x different than DDR2 controller on ADSP-2146x ?

    ADSP-2146x

    ADSP-SC58x/ADSP-2158x

    Supports only DDR2 memory devices Supports DDR3, DDR2, and LPDDR memory devices
    Supports maximum clock/data rate of 225/450 MHz Supports maximum…
  • ADSP-SC5xx/ADSP-215xx

    EngineerZone technical forum that provides customer support for Analog Devices ADSP-SC5xx/ADSP-215xx products.
  • Is there any provision to program the CLKIN frequency input to the ADSP-SC59x/ADSP-2159x processor with software?

    Is there any provision to program the CLKIN frequency input to the ADSP-SC59x/ADSP-2159x processor with software?