• On-chip flash for ADSP-BF538F and ADSP-BF539F

    It is mentioned in the data sheet that we need to connect /AMS0 to /FCE to boot
    from on-chip flash.  What should be done with the /FRESET pin?

     

    Typical applications using the Spansion flash device externally would tie
    /FRESET to the system…
  • ADSP-BF538F SPI0 INTEFACING

    Hello guys,

    I am working on configuring a slave device with ADSP-BF538F and I am able to generate SPI clock and Slave select. The isssue is that I find no signal getting generated on the MOSI pin. I checked the return value of submitbuffer function which…

  • Pin Muxing in CCES 1.1.0 for ADSP-BF538F

    Hi All,

    I am using the black fin processor ADSP-BF538F in one of our project. I am using the cross core embedded studio 1.1.0 IDE for my development. I followed the procedure to create a cross core project as per the training videos and I observed that…

  • RE: BF538F EZ KIT Flash Programming

    Try following the POST code read me exactly as it is - the code is usually a diagnostics test for evaluation board:

    C:\Program Files\Analog Devices\VisualDSP 5.0\Blackfin\Examples\ADSP-BF538F EZ-KIT Lite\Power_On_Self_Test

    Regards

    Prasanth

  • Starting with the BF538F EZ KIT

    Hi,

    I just got a BF538F ez kit lite and am trying to figure out how to use it. I'm trying to start just by controlling some GPIO pins. After looking through the ADSP-BF538F BF processor hardware reference I found the GPIO registers I need to use (PORTCIO_FER…

  • RE: BF538F - On-chip Flash

    Hi,

    regarding your third question, this is explained in the readme for the Flash Programmer Driver at: "...\Blackfin\Examples\ADSP-BF538F EZ-KIT Lite\Flash Programmer\InternalFlash\"

    For your convenience:

    "If you take a look at the datasheet…

  • Minimal Requirement for Building uClinux for Blackfin BF538F

    Hi,

    Hope you are doing fantastic.

    I am having a query, could anybody tell me what are the minimum hardware requirements with Black Processor (ADSP-BF538F) in order to port and run uCLinux.

    Major components interfaced with Blackfin are SDRAM, AD9364  and…

  • BF538F EZ KIT SCLK

    Hi,

    I'm using a BF538F EZ KIT and am trying to figure out sclk and cclk.  The EZ KIT supplies the blackfin processor with an input clock (maybe I can find this value in the BF538F EZ-KIT Lite Hardware Reference Manual?).  And I should use the PLL registers…

  • BF538F EZ KIT Timers

    Hi,

    I'm using the BF538F EZKIT and am trying to sample from an external device every 960Hz.  I'm trying to set up the core timer to toggle an LED on the EZKIT board to see if it's working.  Using the core timer registers in the HRM:

    TCNTL…

  • BF538F EZ KIT UART

    Hi,

    I'm trying to use UART0 to transmit from the BF358F EZ KIT to a PC with the following settings: 8 data bits, 1 stop bit, no parity, LSB first and a baud rate calculated as: baud rate = sclk/(16 * divisor), where 1< divisor < 65536. 

    I…