Hi all,
I'm pleased to announce that we have released a public beta of the 2.0 release of Yocto Linux for ADSP-SC5xx.
The beta release currently contains support for the following development boards:
Other boards will be added…
What are the differences between EMAC on ADSP-SC598 processor family as compared to ADSP-SC594 processor family?
2011-06-20 16:38:35 L1 bf532 error compiling
Wilson Cifuentes (COLOMBIA)
Message: 101496
I have a problem, I compiled the kernel to work with image acquisition using ffmpeg, but when running the application as it says in:
It is an error, which…
2009-09-10 22:44:04 Usb failed on uclinux2009r1-rc6 on bf532 board
roy xue (CHINA)
Message: 79759
Hi,all
I'm try to use sl811-hcd for usb on 532 board. but there is oops when insert the usb device.
----------------------------------------…
What version of Pads do you need to view the pcb files and schematics of the ADSP-SC589 EZ-KIT evaluation board that you provide for this board .
Regads
Athanasios
I want to check the internal ram using the March C algorithm。The question is the March C algorithm will destroy the data in ram and will casue the program running and flying.
usually,this test can be placed in the startup file,but the sharc processors…
Hi
Would you pls help to check below question., thanks
1)Does it need special configuration for SPORT1 ? or there is referance code ? it' can't work when refer SPORT0、2、3 configuration that SPORT0、2、3 can work .
2) Can DAI0 data be routed to DAI1 output…
Hi
Would you pls help to check below question., thanks
1)Does it need special configuration for SPORT1 ? or there is referance code ? it' can't work when refer SPORT0、2、3 configuration that SPORT0、2、3 can work .
2) Can DAI0 data be routed to DAI1 output…