Hi,The ADSP-BF527 is in production and ADSP-BF527F EZ-Kit Lite evaluation hardware provides a low-cost hardware solution for evaluating the ADSP-BF52x Blackfin processor family.Please find the below link which you can refer to get more information on…
We use ADSP-BF527 as a data buffer and protocol converter between a data collection system and USB.
It is connected in peripheral mode.
It is transferring a stream of data as blocks of 512 byte data with 4 or five blocks every 0.5 milliseconds.
It…
Hi
We have a ADSP-BF527 target board. We are compiling a baremetal C application and the log is below. But the libgloss stubs are not present and we get lot of warnings.
After some more hunting in the toolchain we find that under 2011R1-BETA1/binutils…
With ADSP BF527 via ICE-100B and VisualDSP++ 5.0 update 10 ...
1. how long should Flash/Programming/Program take for an M25P64 (Erase all/Intel Hex/Verify while programming)?
2. how long should Flash/Programming/Compare take for an M25P64?
3. how long…
Hi CraiG, thanks for the answer.
I haven't tested on a real Windows environment yet, but this behaviour is not seen on any other USB devices I pug the same way.
The data are:
Board Revision : ADSP-BF527 EZ-KIT LITE 2.0 ( the 2.0 is on a sticker…
Im new to VisualDSP++ and Blackfin processors, so im seeking some help.
I started working with the ADSP-BF527 EZ-KIT LITE 1.5, and I have to make a userinterface on the LCD. My problem is, I can't figure out how to write characters to the display…
I have a problem with the ADSP-BF527 EZ-KIT LITE 1.5.
I was working on getting the audio codec running in VDK, and suddenly the backlight to the display was gone. I tried running the "Power On Self Test" and it was initializing correctly and blinking…
Sir
Can you please guide me in what way I can interface Blackfin ADSP BF527 with Labview. I know labview supports Blackfin processors, but i am not able to connect my board to labview and program it as my way. I tried a lot of ways to make communication…
Hi Team,
We using BF527 ez-kit rev2.2,we changed boot mode and return back to default mode(Mode1),but we didn't get factory default mode.so try reset to starting position and follow POST parallel in VDSP foder path C:\Program Files\Analog Devices\VisualDSP…
Im working on getting the codec to work in VDK. I have used the example "AudioCodec" from the drivers folder in ADSP-BF527 folder and ported it to VDK. But when I run the code I get the error:
Failed to set dataflow method, Error Code:…